Hi, Expert :
I have download Linux SDK, and I find two u-boot.img in SDK
one is in A53 folder:
ti-processor-sdk-linux-automotive-j7-evm-07_00_01\board-support\u-boot_build\a53\u-boot.img
another one is in R5 Folder :
ti-processor-sdk-linux-automotive-j7-evm-07_00_01\board-support\u-boot_build\r5\u-boot.img
What's the difference between these two u-boot.img?
And which one for boot in "boot partition" (eMMC/SDCARD)?
If I need to debug u-boot by CCS, What's the file I should load in CCS
Many Thanks
Gibbs