This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-DRA7X: Linux SDK dra7xx-evm-vision.dtb Missing

Part Number: PROCESSOR-SDK-DRA7X

I am trying to use a DRA7xx-EVM kit with a VisionSuper28 breakout board to access the video input from the HMDI transceiver on the VisionSuper28 daughter board. The DRA7xx-EVM kit is running the default image/filesystem from the v6.00.00.03 automotive Linux SDK. In the SDK developers guide, it says that a specific device tree blob file needs to be select to allow for the vision device drivers to be selected by U-Boot. However, the file that the dev guide specifies (dra7-evm-vision.dtb) does not exist in the rootfs generated by the SDK. Does any one know where I can get the correct device tree blob, or if that fails, the drivers themselves to manually install?

Thanks