Hi all,
I'm trying to build a breakout-board that can employ up to 8 SD cards. I want to implement a simple wav-recorder using the RTC to start recording every hour for about ten minutes. If one of the SD Cards is full, the next card will be used for recording.
My questions are:
1.) How do I connect a single SD Card to the MMCSD Port of the 5505? What is the correct pin connection between SD and 5505?
2.) How can I switch between different cards?
3.) Are there any examples of wav-recording?
By the way I'm queit at the beginning of my ezDSP experiences ;-)
Thanks in regard,
Mo