Other Parts Discussed in Thread: TIDEP0028, TMDSICE3359
Hello,
a post on this forum under [1] states that POWERLINK support for the AM3359 based on openPOWERLINK was implemented in the past.
Unfortunately, i was not able to find any further information on that on the forum or on the web. TIDEP0028 [2] and TIDUA75 [3] state that support for POWERLINK is available but i can't find a link to any implementation other than a commercial solution offered by Port.
So my questions are:
- Was the support using openPOWERLINK stated in [1] ever implemented and is it available as open source?
- If not, are there other open source reference implementations to test POWERLINK on AM335x, for example on the TMDSICE3359 board?
As a research project, we are evaluating hardware platforms which can be used for POWERLINK (particularly openPOWERLINK) in combination with microkernel operating systems.
Any further information or hints to a reference implementation are highly appreciated.
Thanks and best regards!
Johannes Wiesboeck
[1] https://e2e.ti.com/support/processors/f/791/p/700757/2598072#2598072