I am trying to flash the NAND with the WinCE operating system on the LogicPD OMAP-L138 EVM in order to do a standalone boot. As I could not find any instructions to accomplish this I followed the instructions for booting from SD card, substituting NAND flash where appropriate. Using the sfh_OMAP-L138 serial flasher host I flashed EBOOTNANDFLASH.nb0 into the nand flash and that all worked fine. I then copied the NK.nb0 file from the release folder to the NAND flash folder using the explorer app. The boot NK from NAND fails and it reverts to booting from EMAC as shown below. What am I doing wrong that is causing the error "ERROR: BLFlashDownload: Image Signature not found 0x0 != 0x43454345"?
Boot log:
-----------
OMAP-L138 initialization passed!
Booting TI User Boot Loader
UBL Version: 1.65
UBL Flashtype: NAND
Starting NAND Copy...
Valid magicnum, 0x55424CBB, found in block 0x00000006.
DONE
Jumping to entry point at 0xC7F60000.
01
Microsoft Windows CE Bootloader Common Library Version 1.4 Built Feb 18 2011 08:50:31
INFO:OALLogSetZones: dpCurSettings.ulZoneMask: 0xb
Microsoft Windows CE EBOOT 1.0 for OMAPL138 OMAPL138/AM18X EVM. Built Feb 18 2011 at 08:54:46
BSP version 1.3.0, SOC version 1.3.0
CODE : 0xC7F60000 -> 0xC7FA0000
DATA : 0xC7FA0000 -> 0xC7FE0000
STACK : 0xC7FE0000 -> 0xC8000000
Enabled OAL Log Zones : ERROR, WARN, INFO,
Platform Init done
System ready!
Preparing for download...
Predownload...
Valid boot configuration found
Read production data: done
Lan MAC: 00:08:ee:03:6e:a0
INFO: MAC address: 00:08:ee:03:6e:a0
WARN: Invalid BSP_ARGS data found (using defaults)
WARN: Unable to get hardware entropy
Hit space to enter configuration menu 0
Device ID set to OMAPL138-28320
BLFlashDownload: LogicalLoc - 0x62000000
Load NK image from flash memory (NAND)
ERROR: BLFlashDownload: Image Signature not found 0x0 != 0x43454345
MAC addr is 0:8:ee:3:6e:a0.
OMAPEmacInit: f_pEmacRxDesc = 0x1e20000
OMAPEmacInit: f_pEmacTxDesc = 0x1e21000
OMAPEmacInit: waiting for active phy...
OMAPEmacInit: f_pMdioRegs->m_Alive = 0x1
INFO: Boot device uses MAC 00:08:ee:03:6e:a0
InitDHCP():: Calling ProcessDHCP()
ProcessDHCP()::DHCP_INIT
Got Response from DHCP server, IP address: