Part Number: PROCESSOR-SDK-OMAPL138
Other Parts Discussed in Thread: OMAPL138
Hello,
I am using OMAPL138 LCDK board.
processor sdk "pdk_omapl138_1_0_8". I have program for ARM and DSP. Both the programs working fine with the Debugger niow I need to put it in bootloader.
I create the bootloader using the below procedure
"processors.wiki.ti.com/.../OMAPL138_StarterWare_Booting_And_Flashing
I didnt face any error while flashing the omapl138 board. But after flashing, the program is not working as bootload.
Note:
I have already did boodtoader program for C6748 device which is working perfectly. But I am not able to do it for OMAPL138 device
Kindly help me for checkpoints which I need to look when I flash the bootloader program
Thanks & Regards
Navaneetha krishnan