Using dvsdk 4, DMAI, and the dm368. When I switch to single shot mode in the boot parameters, setting onTheFly capture parameter to false, and asking for UYVY instead of 420SEMIP I get an error from the capture driver as follows....
vpfe_capture: error: should use ipipe
It appears that I can capture frames. I wrote them to a file and intend to write an app to check them out to see if they are correct. But I was wondering if this error is incorrect and should be ignored. Or does it point to something I need to fix?
The reason for my configuration is that I need to capture and encode the frames interlaced. Or even capture them interlaced and use a better algorithm to deinterlace before encoding. Both actually since I need to deinterlace then rescale to SIF sized videos and the demo version of dropping fields is entierly unacceptable quality.
John A