Hi,
We are using a leopard board from leopardimaging based on DM365. We would like it to display images on an LCD. The board has a 50 pin connector for LCD interface. The specification says its a 16-bit LCD interface (which I assume is 565). Can I hook it with a 18-bit LCD? In particular I am considering Sharp LCD LQ043T3DX02.
Please let me know if this LCD will be compatible with DM365 LCD output?
Thanks,
Niranjan