Part Number: AM5728
Other Parts Discussed in Thread: TSC2046
Hi Expert
In kernel our tsc2046 is working on MCSPI2 fine, but we would like to read it by sspi cmd in U-boot.
The cmd sspi is not working,
Hit any key to stop autoboot: 0 => => sspi 2:0.0 16 d0 Invalid bus 2 (err=-19) =>In \u-boot-2018.01\arch\arm\dts\am571x-idk.dts we have aliases { spi0 = &mcspi2; }; &mcspi2 { status = "okay"; ti,pindir-d0-out-d1-in; tsc2046@0 { interrupt-parent = <&gpio1>; interrupts = <25 0>; /* gpio1_25=25 */ pendown-gpio = <&gpio1 25 GPIO_ACTIVE_HIGH>; reg = <0>; /* CS0 */ compatible = "spidev"; spi-max-frequency = <1500000>; vcc-supply = <&ldousb_reg>; ti,x-min = /bits/ 16 <0>; ti,x-max = /bits/ 16 <8000>; ti,y-min = /bits/ 16 <0>; ti,y-max = /bits/ 16 <4800>; ti,x-plate-ohms = /bits/ 16 <40>; ti,pressure-max = /bits/ 16 <255>; ti,swap-xy; wakeup-source; }; }; In u-boot-2018.01\configs\am57xx_evm_defconfig we have CONFIG_DM_SPI=y CONFIG_TI_QSPI=y In u-boot-2018.01\arch\arm\mach-omap2\omap5\hw_data.c we have void enable_basic_clocks(void) + (*prcm)->cm_l4per_i2c2_clkctrl, + (*prcm)->cm_l4per_mcspi2_clkctrl, void enable_basic_uboot_clocks(void) + (*prcm)->cm_l4per_mcspi2_clkctrl,