Hi everyone!
I have a simple question, in example, evm6747,mmcsd is necesary utilize Linux, or you can just run this program and have a new file in the sd card?
Best regards,
Paulina
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi everyone!
I have a simple question, in example, evm6747,mmcsd is necesary utilize Linux, or you can just run this program and have a new file in the sd card?
Best regards,
Paulina
Hi Paulina,
I guess you are using the BIOS PSP 1.30.01, if so then the sample application provided with the package only does read/write in raw mode. So no file is created in the SD card.
The sample application writes block of data bytes and reads it back and verifies the data read.
Please refer section 13.11 of C6747_BIOSPSP_Userguide document.
Thanks and Regards,
Sandeep K