Hello,
I would like to ask one question on the speed of DM6437 on EVM6437.

Because
1. From slvs412d, the SWIFT regulator document, I found the formula for calculating output voltage.
2. From evm6437 schematics, I found the value of resistors determining DSP_CORE_VDD. Substituting these values into the formula, the output voltage is 1.05V.
3. From evm6437 tech reference, it appears that its DSP can operate at maximum 600MHz, so I presume it is of the -6 device.
From SPRS345d, 5.2 Recommended Operating Conditions, -6 device at 1.05V runs at 450MHz.
Is this result correct? If yes, then 450MHz is pretty low in the column, why the EVM picks this value?
Thanks,
Zheng