This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I want to check if R5F's Instruction and Data Cache is enabled or not.
Attaching the System Register. Please help me check if I can get the above information from the System Registers:
Hi Linda Xie,
If you check the R5F TRM (https://developer.arm.com/documentation/ddi0460/c/System-Control/Register-descriptions/c1--System-Control-Register?lang=en ) section 4.3.16 c1, System Control Register, you will see the following:
1. 12th Bit (I bit) determines if the I cache is enabled or not
2. 2nd Bit (C bit) determines if the D cache is enabled or not
This register can be read from CCS via the Register -> System registers -> CP15_SYSTEM_CONTROL register.
For you application, I see the value as 0x00E5187D - here both the I and the C bits are 1, hence we can confirm that the I cache and the D cache are both enabled.
On a side note, there is an implementation for the SYSBIOS code at bios_6_83_00_18\packages\ti\sysbios\family\arm\v7r\Cache_asm.sv7R - see ti_sysbios_family_arm_v7r_Cache_getEnabled__E , ti_sysbios_family_arm_v7r_Cache_enableL1d__I and ti_sysbios_family_arm_v7r_Cache_enableL1p__I functions.
The above mentioned functions also try to get the status of the I and D caches which in this case we are viewing from the CCS System Registers View.
Regards,
Karan
Hi,Karan
Thank you very much for confirming this information for me, it is very useful to me, thanks again!
Regards,
Xie