Hi,
using the PSDK LINUX and RTOS v7.1 with the default filesystem and kernel, I am trying to bring-up the network interface for the CPSW9g. Currently only the CPSW2g network interface is working, which is eth0 on MCU ENET port on the EVM.
But the board has also the 4x Ethernet port board connected with the QSGMII PHY, which is connected on the CPSW9g.
The ethernet switch firmware is loading correctly
root@j7-evm:/sys/class/remoteproc/remoteproc4# echo "start" > state
[ 9238.065327] remoteproc remoteproc4: powering up 5c00000.r5f
[ 9238.073082] remoteproc remoteproc4: Booting fw image j7-main-r5f0_0-fw, size 4839748
[ 9238.080994] platform 5c00000.r5f: R5F core initialized in IPC-only mode
[ 9238.087624] remoteproc4#vdev0buffer: assigned reserved memory node r5f-dma-memory@a1000000
[ 9238.096377] virtio_rpmsg_bus virtio3: rpmsg host is online
[ 9238.102841] remoteproc4#vdev0buffer: registered virtio3 (type 7)
[ 9238.109038] remoteproc remoteproc4: remote processor 5c00000.r5f is now up
The virtual MAC driver is loading
j721e_cpsw_virt_mac 327680 0
The rpmsg driver is also loading
rpmsg_kdrv_switch 262144 0
Should we not see something like an eth1 for the CPSW9g?
Thanks!
--Gunter