Dear:
I used tidl import tool to generate bin file. With the bin file generated, I run the avp app demo, but there is an error as below:
VX_ZONE_ERROR:[tivxAlgiVisionCreate:331] Calling ialg.algAlloc failed with status = -1115
The bin file I generated only about 700KB, so I don't think this error caused by lacking of memory.
There is my convert model param configuration:
modelType = 0
inputNetFile = "./segment_forward/deploy_768x384.prototxt"
inputParamsFile = "./segment_forward/forward_768x384_iter_60000.caffemodel"
outputNetFile = "./segment_forward/tidl_net_jSegNet21v2_768x384.bin"
outputParamsFile = "./segment_forward/tidl_io_jSegNet21v2_768x384_"
inDataFormat = 0
perfSimConfig = ./segment_forward/perfsim_base.cfg
inData = "../../test/testvecs/config/segmentation_list.txt"
postProcType = 3