Hi again,
Currently I use the C5515. In my application it might be of great benefit to have DMA on the GPIO I/O space in order to have autonomous data transfer between DSP and an external device.
My question is : is there a DSP in the C55x family which can provide DMA to GPIO I/O space, or even better a DSP with:
- either two 2 SPI running at fCLK = 32 MHz with DMA or
- 4 SPI running at fCLK = 16 MHz with DMA
Or what other combination of DSP/peripheral can provide 4 autonomous channels with at least 16 Mbps per channel?
According to an old post from me (http://e2e.ti.com/support/dsp/tms320c5000_power-efficient_dsps/f/109/p/74661/272875.aspx#272875) the problem is that the C5515's DMA cannot access neither GPIO I/O nor SPI I/O space.
Can the C5509 or the C5505 do this?
Thank you very much for your answers.
Andreas