The values in Table 5-3 of the datasheet for AM 572x family (SPRS953G) provide the POH values for some combinations of temperatures/modes of operation.
For some applications this may be sufficient if the system has enough forced air flow. However if the air flow is restricted or only passive cooling is available would be benefic to chose deviate from these conditions and achieve maximum performance possible for that specific situation.
As an example:
- the system doesn't run the DSP, IVA, GPU, HDMI, PCI
- ARM CPU at 1.5GHz uses only USB 2.0 and PRU (GMAC and PRU ETH)
The cooling conditions for the application are creating a TJ that by the table 5-3 gives a too low POH number.
In a simplistic scenario if the ARM core would be running at lower speed (somewhere between 1.5 and 1.176) what would be the TJ - POH relation (this assume VDD_MPU is OPP_HIGH)
In a more complex scenario VDD_MPU can be lowered towards OPP_OD to achieve even better CPU performance or higher POH.