Part Number: TDA2EG-17
Hi,
SDK: ti-processor-sdk-linux-automotive-dra7xx-evm-03_04_00_03
uboot:
VERSION = 2016
PATCHLEVEL = 05
In the DDR configuration file avatar_ EMIF_ RegisterConfigt.xlsm If the "leveling technique:" s / W "in" is set to HW, why can't there be any output and start? If it is set to SW, uboot can start normally.
I have compared the differences between HW and SW in the following aspects:
Sw:
.emif_ Rd_ Wr_ lvl_ rmp_ ctl = 0x00000000,
.emif_ ddr_ phy_ ctlr_ 1_ init = 0x0E24400F,
Hw:
.emif_ Rd_ Wr_ lvl_ rmp_ ctl = 0x80000000,
.emif_ ddr_ phy_ ctlr_ 1_ init = 0x0824400F,
Is tda2eg-17 supported HW ?