Part Number: 66AK2E05
We do not plan to use Hyperlink in a design underway. I'm looking for best practices on what to do with the unused interface in hardware.
- Clock: HYPLNK0CLKP/N
- Currently I do not have a clock driven to this interface.
- Is this acceptable or could it lead to crashes/lockup if the peripheral is accessed?
- Should the pins be NC, Pull Up, Pull Down, something else?
- Interface:
- Should the pins be NC or tied to something for lowest power?
- I assume the HYPLNK0RESREF (3.0k, 1% to GND) is still required for safe operation.