Hello.
Does C6746 support frequency as 375MHz/456MHz?
The current datasheet of C6746 describes that C6746 support 300MHz.
I think this is old information.
Best regards, RY
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Yes, the C6746 will also supports 375 MHz / 456 MHz. The datasheets are currently being revised as such.