Part Number: AM4382
Hi,
This is Pankaj from eInfochips India and I am currently working on AM4382CZDNA30S Processor Based Project which is used for EPOS application and we are using TPS65218D0RSLR PMIC with the AM4382CZDNA30S Processor and my system is battery (3.7V@2500maH) as well as 5V External DC supply operated and we have IRIS, RGB Camera, wifi, BLE Barcode scanner and Finger Print sensor Interface on Board and now we are facing two major issues as:
1.Board Reboot Issue over Battery: As in this issue when we are discharging battery over the use case: IR LEDs, IRIS camera, WIFI, Display continuous ON then after some time my board gets reboot and this shall occurs very randomly like during discharging sometimes it came on battery drained at 50 percent and sometimes it came on battery drained 30 percent.
2.Processor Damage Issue: We have observed in three boards as VDD_CORE_1.1V core supply and VDDSHV_3V3 of processor gets short with ground. In this case we try to find all possible reasons but we didn't got any technical reason due to that the board get damaged so could you let us more about this processor sensitivity as is very sensitive towards ESD or required any other special care instructions or is there any such related problems with this processor earlier.
Regards,
Pankaj Kanthaliya