Other Parts Discussed in Thread: SYSBIOS
Customer trying to resurrect and modify old code. Was asked to bring this section to the Processor forum
Running into the following errors
We tried to convert the old CCS v2 project to CCS v8 project but lot of errors are coming due to supporting files missing.
We need to convert this project to CCS v8 without an error please let me any process to convert this project without any errors.
Below is the compilation error we got while converting from CCS v2 project to CCS v8.
>> Compilation failure
subdir_rules.mk:9: recipe for target 'C:/ti2/myprojects/CIC1008-1V1.18/Debug/C6712.obj' failed
"C:/Users/skola/workspace_v8/AC/std.h", line 87: fatal error #5: could not open source file "ti/targets/select.h"
1 fatal error detected in the compilation of "../C6712.c".
Compilation terminated.
gmake: *** [C:/ti2/myprojects/CIC1008-1V1.18/Debug/C6712.obj] Error 1
Building file: "../EVENT.C"
>> Compilation failure
subdir_rules.mk:65: recipe for target 'C:/ti2/myprojects/CIC1008-1V1.18/Debug/STA.obj' failed
"C:/Users/skola/workspace_v8/AC/stdlib.h", line 88: fatal error #5: could not open source file "__config"
1 fatal error detected in the compilation of "../STA.C".
Compilation terminated.
gmake: *** [C:/ti2/myprojects/CIC1008-1V1.18/Debug/STA.obj] Error 1
Building file: "../Sta_ape.c"
Invoking: C6000 Compiler
We would like to get a McBSP project example running on CCSv2 also, So that we can make it as our reference and compare with our project for missing files.