Part Number: J721EXSOMXEVM
Other Parts Discussed in Thread: TDA4VM
I have some problems with boot Linux from SD-card on TDA4VM board.
I tried to install PSDKLA 07_00_01_01 following your instruction at https://software-dl.ti.com/jacinto7/esd/processor-sdk-linux-jacinto7/latest/exports/docs/linux/Overview/Run_Setup_Scripts.html, but after installation with all defaults from your script I suppose that something gone wrong.
Now, I cannot boot from prebuilt SD-card from your delivery set after incorrect installation of0 PSDKLA.
Now, I have 2 main problems:
1) Can not reinstall PSDKLA on host via setup.sh because of u-boot abort (see u-boot log below) and no access to tftp.
2) Cannot load OS from sd-card backup. Backup restore on sd-card has no effect for u-boot – same error of Bad Linux image.
Current boot log is:
Welcome to minicom 2.7.1 OPTIONS: I18n Compiled on Aug 13 2017, 15:25:34. Port /dev/ttyUSB0, 21:13:01 Press CTRL-A Z for help on special keys ........................................... U-Boot SPL 2020.01-gf9b0d030d3 (Jun 17 2020 - 15:08:08 +0000) SYSFW ABI: 3.0 (firmware rev 0x0014 '20.04.1-v2020.04a (Terrific Lla') Trying to boot from MMC2 Loading Environment from MMC... *** Warning - No MMC card found, using default t Remoteproc 2 started successfully Starting ATF on ARM64 core... NOTICE: BL31: v2.3():07.00.00.005-dirty NOTICE: BL31: Built : 14:33:55, Jun 17 2020 U-Boot SPL 2020.01-gf9b0d030d3 (Jun 17 2020 - 14:34:25 +0000) SYSFW ABI: 3.0 (firmware rev 0x0014 '20.04.1-v2020.04a (Terrific Lla') Detected: J7X-BASE-CPB rev E3 Detected: J7X-VSC8514-ETH rev E2 Trying to boot from MMC2 U-Boot 2020.01-gf9b0d030d3 (Jun 17 2020 - 14:34:25 +0000) SoC: J721E SR1.0 Model: Texas Instruments K3 J721E SoC Board: J721EX-PM2-SOM rev E7 DRAM: 4 GiB not found for dev hbmc-mux Flash: 0 Bytes MMC: sdhci@4f80000: 0, sdhci@4fb0000: 1 Loading Environment from MMC... OK In: serial@2800000 Out: serial@2800000 Err: serial@2800000 Detected: J7X-BASE-CPB rev E3 Detected: J7X-VSC8514-ETH rev E2 Net: eth0: ethernet@046000000 Hit any key to stop autoboot: 0 switch to partitions #0, OK mmc1 is current device SD/MMC found on device 1 0 bytes read in 1 ms (0 Bytes/s) Loaded env from uEnv.txt Importing environment from mmc1 ... ethernet@046000000 Waiting for PHY auto negotiation to complete................e link up on port 1, speed 1000, full duplex BOOTP broadcast 1 BOOTP broadcast 2 DHCP client bound to address 10.10.10.49 (525 ms) link up on port 1, speed 1000, full duplex BOOTP broadcast 1 DHCP client bound to address 10.10.10.49 (275 ms) link up on port 1, speed 1000, full duplex *** ERROR: `serverip' not set link up on port 1, speed 1000, full duplex *** ERROR: `serverip' not set libfdt fdt_check_header(): FDT_ERR_BADMAGIC No FDT memory address configured. Please configure the FDT address via "fdt addr <address>" command. Aborting! Bad Linux ARM64 Image magic!
Tried to set IP has no effect.
Can anyone suggest a solution?