This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-AM335X: Ethernet Booting

Part Number: PROCESSOR-SDK-AM335X
Other Parts Discussed in Thread: AM3358

Hi!

I am using Sitara AM3358 processor on custom board.

My client needs to flash the code through Ethernet. For this, processor has to boot through Ethernet. Could you help me in this matter?

Is there any GUI required or any Ethernet Bootloader is there?

Secondly, client wants to control the booting either through RS422 or Ethernet to flash the code. As I can see in TRM there is no option available in which all booting devices(UART, Ethernet, NAND) are available. We can't put switches to the unit due to some safety standards. Is there any solution for this?

Regards,

Gaurav