This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: About TISCI X509 Certificate System Firmware Debug Extension

Part Number: TDA4VM


In the TISCI X509 certificate system firmware debug extension, The structure of the field is shown below in ASN.1 notation.

UID-Debug ::= SEQUENCE​{     

    uid OCTET STRING, -- unique ID of the device for which this certificate applie   

    debugCtrl INTEGER, -- debug control information     

    coreDbgEn INTEGER, -- Core IDs for which debug must be enabled     

    coreDbgSecEn INTEGER, -- Core IDs for which secure debug must be enabled​

}

The debug control data is decoded as a structure below:

struct sdbg_debug_ctrl {

    u16 debug_priv_level;

    u16 hw_key_hide_flags;

    u8 debug_core_sel[MAX_CPU_CORES];

    u8 sec_debug_core_sel[MAX_CPU_CORES];

}

Whether debugCtrl, coreDbgEn, coreDbgEn form struct sdbg_debug_ctrl,In other words,

debugCtrl={u16 debug_priv_level; u16 hw_key_hide_flags};

coreDbgEn=debug_core_sel[MAX_CPU_CORES];

coreDbgSecEn=sec_debug_core_sel[MAX_CPU_CORES];

Is that right?

If so, then MAX_CPU_CORES=4; Why is the maximum number of CPU cores only 4?

In addition, is the certificate format used by TISCI_MSG_OPEN_DEBUG_FWLS der or pem?