Part Number: AM4378
Hello Champs,
Customer designed his own AM4378 board and failed to boot from SD card.
1. Creating SD card, the SD card could boot from AM437x_gpEVM and Rico Board AM4378
2. Insert SD card to customer board, it can't boot, no output from UART0.
a. Have configured sysboot pin to SD boot mode.
b. input clock is 24M
c. There is 250KHz clock from SD clk pin, CMD(Pin3) and Data0(Pin7) is high without wave
d. If setting sysboot pin to uart boot mode, there is CCCC.....outputting from UART0.
What's the problem?
Thanks.
Rgds
Shine