Hello All
I am using DM648 with Hello World Application of NDK2.0 want to write some bytes to NOR flash during the program execution. Plz refer with some examples.
Regards
Mark
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello All
I am using DM648 with Hello World Application of NDK2.0 want to write some bytes to NOR flash during the program execution. Plz refer with some examples.
Regards
Mark
This does not actually seem to be a BIOS or NDK issue, so I am going to move it to the DM64x forum to hopefully get it a faster response.
Dave
There is an example in TI dvsdk itself. The demo provided in the dvsdk includes the source code and a small application to program it in flash memory with source code. See instructions under:
"C:\dvsdk_x_xx_xx_xx_DM648\flashutil\DM648 EVM Flashing and Booting Instructions.doc"
Replace C:\dvsdk_x_xx_xx_xx_DM648 with TI dvsdk installation path.
Sriram
I already had done work on this code you mentioned several times but this allows you only to burn the complete nor flash with UBL.ais and UserProject.ais however i just want to write few bytes in NOR flash at some specific locations i just need that.
Here is the response from Lyrtech Inc:
[Lyrtech] Programming a whole file or only few bytes can be done with the same routines. Just don't forget that you will have to erase a complete flash sector before programming your few bytes (so it would not erase one byte at a time, but a bunch of them)
Regards, Srirami.