Hi,
Is that possible to read the actual device speed?
As per SPRS691E, the device speed register (DEVSPEED) register 0x026203F8 has
31-23 DEVSPEED Indicates the speed of the device (read only)
0000 0000 0b = 800 MHz
0000 0000 1b = 1000 MHz
0000 0001 xb = 1200 MHz
0000 001x xb = 1250 MHz
0000 01xx xb = 1400 MHz
0000 1xxx xb = 1400 MHz
0001 xxxx xb = 1250 MHz
001x xxxx xb = 1200 MHz
01xx xxxx xb = 1000 MHz
1xxx xxxx xb = 800 MHz
The description says "The Device Speed Register depicts the device speed grade", this may not be the actual device speed but the capability if I understand correctly.
Why there are two bits for same speed?
Is there any register that will show the actual speed?
Please clarify
Thanks