Part Number: TDA4VM
Hi,
After flashing eMMC according to the thread https://software-dl.ti.com/jacinto7/esd/processor-sdk-linux-jacinto7/latest/exports/docs/linux/How_to_Guides/Target/How_to_flash_emmc_device.html ,I try to load it manually from u-boot in the TDA4VM EVM.But I can't run the application as I do it in SD boot mode.I will post the boot log below .Can you help me solve it?
Regards!
HJ
U-Boot SPL 2020.01-gf9b0d030d3 (Jun 17 2020 - 15:08:08 +0000)
SYSFW ABI: 3.0 (firmware rev 0x0014 '20.04.1-v2020.04a (Terrific Lla')
Trying to boot from MMC1
Loading Environment from MMC... *** Warning - bad CRC, using default environment
init_env from device 17 not supported!
Loading rproc fw image from device 17 not supported!
Loading rproc fw image from device 17 not supported!
Starting ATF on ARM64 core...
NOTICE: BL31: v2.3():07.00.00.005-dirty
NOTICE: BL31: Built : 14:33:55, Jun 17 2020
U-Boot SPL 2020.01-gf9b0d030d3 (Jun 17 2020 - 14:34:25 +0000)
SYSFW ABI: 3.0 (firmware rev 0x0014 '20.04.1-v2020.04a (Terrific Lla')
Detected: J7X-BASE-CPB rev E3
Detected: J7X-VSC8514-ETH rev E2
Trying to boot from MMC1
U-Boot 2020.01-gf9b0d030d3 (Jun 17 2020 - 14:34:25 +0000)
SoC: J721E SR1.0
Model: Texas Instruments K3 J721E SoC
Board: J721EX-PM2-SOM rev E7
DRAM: 4 GiB
not found for dev hbmc-mux
Flash: 0 Bytes
MMC: sdhci@4f80000: 0, sdhci@4fb0000: 1
Loading Environment from MMC... OK
In: serial@2800000
Out: serial@2800000
Err: serial@2800000
Detected: J7X-BASE-CPB rev E3
Detected: J7X-VSC8514-ETH rev E2
Net: eth0: ethernet@046000000
Hit any key to stop autoboot: 0
=>
=> rproc init
=> rproc list
0 - Name:'r5f@41000000' type:'internal memory mapped' supports: load start stop reset
1 - Name:'r5f@41400000' type:'internal memory mapped' supports: load start stop reset
2 - Name:'r5f@5c00000' type:'internal memory mapped' supports: load start stop reset
3 - Name:'r5f@5d00000' type:'internal memory mapped' supports: load start stop reset
4 - Name:'r5f@5e00000' type:'internal memory mapped' supports: load start stop reset
5 - Name:'r5f@5f00000' type:'internal memory mapped' supports: load start stop reset
6 - Name:'dsp@4d80800000' type:'internal memory mapped' supports: load start stop reset
7 - Name:'dsp@4d81800000' type:'internal memory mapped' supports: load start stop reset
8 - Name:'dsp@64800000' type:'internal memory mapped' supports: load start stop reset
=> load mmc 0:2 0x90000000 /lib/firmware/j7-mcu-r5f0_0-fw
190412 bytes read in 5 ms (36.3 MiB/s)
=> rproc load 0 0x90000000 0x${filesize}
Load Remote Processor 0 with data@addr=0x90000000 190412 bytes: Success!
=> rproc start 0
=> load mmc 0:2 0x90000000 /lib/firmware/j7-main-r5f0_0-fw
215396 bytes read in 4 ms (51.4 MiB/s)
=> rproc load 2 0x90000000 0x${filesize}
Load Remote Processor 2 with data@addr=0x90000000 215396 bytes: Success!
=> rproc start 2
=> load mmc 0:2 0x90000000 /lib/firmware/j7-main-r5f0_1-fw
141164 bytes read in 4 ms (33.7 MiB/s)
=> rproc load 3 0x90000000 0x${filesize}
Load Remote Processor 3 with data@addr=0x90000000 141164 bytes: Success!
=> rproc start 3
=> load mmc 0:2 0x90000000 /lib/firmware/j7-main-r5f1_0-fw
141164 bytes read in 5 ms (26.9 MiB/s)
=> rproc load 4 0x90000000 0x${filesize}
Load Remote Processor 4 with data@addr=0x90000000 141164 bytes: Success!
=> rproc start 4
=> load mmc 0:2 0x90000000 /lib/firmware/j7-main-r5f1_1-fw
141164 bytes read in 4 ms (33.7 MiB/s)
=> rproc load 5 0x90000000 0x${filesize}
Load Remote Processor 5 with data@addr=0x90000000 141164 bytes: Success!
=> rproc start 5
=> load mmc 0:2 0x90000000 /lib/firmware/j7-c71_0-fw
6590448 bytes read in 23 ms (273.3 MiB/s)
=> rproc load 8 0x90000000 0x${filesize}
Load Remote Processor 8 with data@addr=0x90000000 6590448 bytes: Success!
=> rproc start 8
=> boot
switch to partitions #0, OK
mmc0(part 0) is current device
SD/MMC found on device 0
16654344 bytes read in 53 ms (299.7 MiB/s)
89857 bytes read in 3 ms (28.6 MiB/s)
## Flattened Device Tree blob at 82000000
Booting using the fdt blob at 0x82000000
Loading Device Tree to 00000000fdda1000, end 00000000fdeb9fff ... OK
Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x411fd080]
[ 0.000000] Linux version 5.4.40-g66cf445b76 (oe-user@oe-host) (gcc version 9.2.1 20191025 (GNU Toolchain for the A-profile Architecture 9.2-2019.12 (arm-9.10))) #1 SMP PREEMPT Wed Jun 17 14:28:47 UTC 2020
[ 0.000000] Machine model: Texas Instruments K3 J721E SoC
[ 0.000000] earlycon: ns16550a0 at MMIO32 0x0000000002800000 (options '')
[ 0.000000] printk: bootconsole [ns16550a0] enabled
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a0000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@a0000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a0100000, size 15 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-memory@a0100000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a1000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@a1000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a1100000, size 31 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-memory@a1100000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a3000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@a3000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a3100000, size 15 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-memory@a3100000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a4000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@a4000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a4100000, size 15 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-memory@a4100000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a5000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@a5000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a5100000, size 15 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-memory@a5100000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a6000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node c66-dma-memory@a6000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a6100000, size 15 MiB
[ 0.000000] OF: reserved mem: initialized node c66-memory@a6100000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a7000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node c66-dma-memory@a7000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a7100000, size 15 MiB
[ 0.000000] OF: reserved mem: initialized node c66-memory@a7100000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a8000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node c71-dma-memory@a8000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a8100000, size 15 MiB
[ 0.000000] OF: reserved mem: initialized node c71-memory@a8100000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000fb000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@fb000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000fb100000, size 15 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-memory@fb100000, compatible id shared-dma-pool
[ 0.000000] cma: Reserved 512 MiB at 0x00000000c0000000
[ 0.000000] psci: probing for conduit method from DT.
[ 0.000000] psci: PSCIv1.1 detected in firmware.
[ 0.000000] psci: Using standard PSCI v0.2 function IDs
[ 0.000000] psci: Trusted OS migration not required
[ 0.000000] psci: SMC Calling Convention v1.0
[ 0.000000] percpu: Embedded 2 pages/cpu s48408 r8192 d74472 u131072
[ 0.000000] Detected PIPT I-cache on CPU0
[ 0.000000] CPU features: detected: GIC system register CPU interface
[ 0.000000] CPU features: detected: EL2 vector hardening
[ 0.000000] Built 1 zonelists, mobility grouping off. Total pages: 47825
[ 0.000000] Kernel command line: console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 mtdparts=47040000.spi.0:512k(ospi.tiboot3),2m(ospi.tispl),4m(ospi.u-boot),128k(ospi.env),128k(ospi.env.backup),1m(ospi.sysfw),-@8m(ospi.rootfs);47034000.hyperbus:512k(hbmc.tiboot3),2m(hbmc.tispl),4m(hbmc.u-boot),256k(hbmc.env),1m(hbmc.sysfw),-@8m(hbmc.rootfs) root=PARTUUID=65cb8b22-02 rw rootfstype=ext4 rootwait
[ 0.000000] Dentry cache hash table entries: 524288 (order: 6, 4194304 bytes, linear)
[ 0.000000] Inode-cache hash table entries: 262144 (order: 5, 2097152 bytes, linear)
[ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
[ 0.000000] software IO TLB: mapped [mem 0xbbff0000-0xbfff0000] (64MB)
[ 0.000000] Memory: 3354112K/3063808K available (9534K kernel code, 776K rwdata, 3840K rodata, 1728K init, 695K bss, 18446744073708737024K reserved, 524288K cma-reserved)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
[ 0.000000] rcu: Preemptible hierarchical RCU implementation.
[ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=2.
[ 0.000000] Tasks RCU enabled.
[ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2
[ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode
[ 0.000000] GICv3: 960 SPIs implemented
[ 0.000000] GICv3: 0 Extended SPIs implemented
[ 0.000000] GICv3: Distributor has no Range Selector support
[ 0.000000] GICv3: 16 PPIs implemented
[ 0.000000] GICv3: no VLPI support, no direct LPI support
[ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000001900000
[ 0.000000] ITS [mem 0x01820000-0x0182ffff]
[ 0.000000] GIC: enabling workaround for ITS: Socionext Synquacer pre-ITS
[ 0.000000] ITS@0x0000000001820000: allocated 1048576 Devices @8c0800000 (flat, esz 8, psz 64K, shr 0)
[ 0.000000] ITS: using cache flushing for cmd queue
[ 0.000000] GICv3: using LPI property table @0x00000008c00c0000
[ 0.000000] GIC: using cache flushing for LPI property table
[ 0.000000] GICv3: CPU0: using allocated LPI pending table @0x00000008c00d0000
[ 0.000000] random: get_random_bytes called from start_kernel+0x2b8/0x438 with crng_init=0
[ 0.000000] arch_timer: cp15 timer(s) running at 200.00MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x2e2049d3e8, max_idle_ns: 440795210634 ns
[ 0.000001] sched_clock: 56 bits at 200MHz, resolution 5ns, wraps every 4398046511102ns
[ 0.008363] Console: colour dummy device 80x25
[ 0.012924] Calibrating delay loop (skipped), value calculated using timer frequency.. 400.00 BogoMIPS (lpj=800000)
[ 0.023593] pid_max: default: 32768 minimum: 301
[ 0.028342] LSM: Security Framework initializing
[ 0.033087] Mount-cache hash table entries: 8192 (order: 0, 65536 bytes, linear)
[ 0.040656] Mountpoint-cache hash table entries: 8192 (order: 0, 65536 bytes, linear)
[ 0.072713] ASID allocator initialised with 32768 entries
[ 0.086241] rcu: Hierarchical SRCU implementation.
[ 0.099206] Platform MSI: gic-its@1820000 domain created
[ 0.104817] PCI/MSI: /interconnect@100000/interrupt-controller@1800000/gic-its@1820000 domain created
[ 0.122252] smp: Bringing up secondary CPUs ...
[ 0.159225] Detected PIPT I-cache on CPU1
[ 0.159250] GICv3: CPU1: found redistributor 1 region 0:0x0000000001920000
[ 0.159260] GICv3: CPU1: using allocated LPI pending table @0x00000008c00e0000
[ 0.159292] CPU1: Booted secondary processor 0x0000000001 [0x411fd080]
[ 0.159349] smp: Brought up 1 node, 2 CPUs
[ 0.188692] SMP: Total of 2 processors activated.
[ 0.193496] CPU features: detected: 32-bit EL0 Support
[ 0.198750] CPU features: detected: CRC32 instructions
[ 0.210439] CPU: All CPU(s) started at EL2
[ 0.214634] alternatives: patching kernel code
[ 0.219722] devtmpfs: initialized
[ 0.227799] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[ 0.237768] futex hash table entries: 512 (order: -1, 32768 bytes, linear)
[ 0.245510] pinctrl core: initialized pinctrl subsystem
[ 0.251295] NET: Registered protocol family 16
[ 0.258410] DMA: preallocated 256 KiB pool for atomic allocations
[ 0.264936] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[ 0.281100] HugeTLB registered 16.0 GiB page size, pre-allocated 0 pages
[ 0.287957] HugeTLB registered 512 MiB page size, pre-allocated 0 pages
[ 0.294715] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
[ 0.303487] cryptd: max_cpu_qlen set to 1000
[ 0.310801] vsys_3v3: supplied by evm_12v0
[ 0.315097] vsys_5v0: supplied by evm_12v0
[ 0.319783] iommu: Default domain type: Translated
[ 0.324934] SCSI subsystem initialized
[ 0.329079] mc: Linux media interface: v0.10
[ 0.333485] videodev: Linux video capture interface: v2.00
[ 0.339101] pps_core: LinuxPPS API ver. 1 registered
[ 0.344171] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.353507] PTP clock support registered
[ 0.357518] EDAC MC: Ver: 3.0.0
[ 0.361257] FPGA manager framework
[ 0.364771] Advanced Linux Sound Architecture Driver Initialized.
[ 0.371361] clocksource: Switched to clocksource arch_sys_counter
[ 0.377705] VFS: Disk quotas dquot_6.6.0
[ 0.381750] VFS: Dquot-cache hash table entries: 8192 (order 0, 65536 bytes)
[ 0.391224] thermal_sys: Registered thermal governor 'step_wise'
[ 0.391226] thermal_sys: Registered thermal governor 'power_allocator'
[ 0.397633] NET: Registered protocol family 2
[ 0.409047] tcp_listen_portaddr_hash hash table entries: 4096 (order: 0, 65536 bytes, linear)
[ 0.417815] TCP established hash table entries: 32768 (order: 2, 262144 bytes, linear)
[ 0.426008] TCP bind hash table entries: 32768 (order: 3, 524288 bytes, linear)
[ 0.433791] TCP: Hash tables configured (established 32768 bind 32768)
[ 0.440527] UDP hash table entries: 2048 (order: 0, 65536 bytes, linear)
[ 0.447416] UDP-Lite hash table entries: 2048 (order: 0, 65536 bytes, linear)
[ 0.454820] NET: Registered protocol family 1
[ 0.459596] RPC: Registered named UNIX socket transport module.
[ 0.465653] RPC: Registered udp transport module.
[ 0.470455] RPC: Registered tcp transport module.
[ 0.475258] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.481842] PCI: CLS 0 bytes, default 64
[ 0.486202] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters available
[ 0.497796] Initialise system trusted keyrings
[ 0.502420] workingset: timestamp_bits=46 max_order=16 bucket_order=0
[ 0.511018] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.517262] NFS: Registering the id_resolver key type
[ 0.522435] Key type id_resolver registered
[ 0.526751] Key type id_legacy registered
[ 0.530848] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[ 0.537811] 9p: Installing v9fs 9p2000 file system support
[ 0.550375] Key type asymmetric registered
[ 0.554561] Asymmetric key parser 'x509' registered
[ 0.559570] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 244)
[ 0.567132] io scheduler mq-deadline registered
[ 0.571765] io scheduler kyber registered
[ 0.576986] pinctrl-single 4301c000.pinmux: 94 pins, size 376
[ 0.583075] pinctrl-single 11c000.pinmux: 173 pins, size 692
[ 0.589244] pinctrl-single a40000.timesync_router: 512 pins, size 2048
[ 0.598363] k3-ringacc 2b800000.ringacc: Failed to get MSI domain
[ 0.604632] k3-ringacc 3c000000.ringacc: Failed to get MSI domain
[ 0.610964] ti-pat 31010000.pat: Found PAT Rev 1.0 with 16384 pages
[ 0.617373] debugfs: Directory '31010000.pat' with parent 'regmap' already present!
[ 0.625356] ti-pat 31011000.pat: Found PAT Rev 1.0 with 16384 pages
[ 0.631774] debugfs: Directory '31011000.pat' with parent 'regmap' already present!
[ 0.639699] ti-pat 31012000.pat: Found PAT Rev 1.0 with 16384 pages
[ 0.646112] debugfs: Directory '31012000.pat' with parent 'regmap' already present!
[ 0.654082] ti-pat 31013000.pat: Found PAT Rev 1.0 with 2048 pages
[ 0.660403] debugfs: Directory '31013000.pat' with parent 'regmap' already present!
[ 0.668321] ti-pat 31014000.pat: Found PAT Rev 1.0 with 2048 pages
[ 0.674642] debugfs: Directory '31014000.pat' with parent 'regmap' already present!
[ 0.684035] Serial: 8250/16550 driver, 10 ports, IRQ sharing enabled
[ 0.696013] brd: module loaded
[ 0.702073] loop: module loaded
[ 0.706850] libphy: Fixed MDIO Bus: probed
[ 0.711210] tun: Universal TUN/TAP device driver, 1.6
[ 0.716640] igbvf: Intel(R) Gigabit Virtual Function Network Driver - version 2.4.0-k
[ 0.724646] igbvf: Copyright (c) 2009 - 2012 Intel Corporation.
[ 0.730714] sky2: driver version 1.30
[ 0.734953] VFIO - User Level meta-driver version: 0.3
[ 0.740572] i2c /dev entries driver
[ 0.744663] sdhci: Secure Digital Host Controller Interface driver
[ 0.750977] sdhci: Copyright(c) Pierre Ossman
[ 0.755640] sdhci-pltfm: SDHCI platform and OF driver helper
[ 0.761888] ledtrig-cpu: registered to indicate activity on CPUs
[ 0.768645] optee: probing for conduit method from DT.
[ 0.773909] optee: revision 3.8 (199fca17)
[ 0.774215] optee: initialized driver
[ 0.782967] NET: Registered protocol family 17
[ 0.787582] 9pnet: Installing 9P2000 support
[ 0.791972] Key type dns_resolver registered
[ 0.796536] registered taskstats version 1
[ 0.800723] Loading compiled-in X.509 certificates
[ 0.809466] k3-ringacc 2b800000.ringacc: Failed to get MSI domain
[ 0.815787] k3-ringacc 3c000000.ringacc: Failed to get MSI domain
[ 0.823480] ti-sci 44083000.dmsc: ABI: 3.0 (firmware rev 0x0014 '20.04.1-v2020.04a (Terrific Lla')
[ 0.848927] random: fast init done
[ 0.881675] davinci-mcasp 2ba0000.mcasp: IRQ common not found
[ 0.889003] omap_i2c 40b00000.i2c: bus 0 rev0.12 at 100 kHz
[ 0.894992] omap_i2c 40b10000.i2c: bus 1 rev0.12 at 100 kHz
[ 0.900947] omap_i2c 42120000.i2c: bus 2 rev0.12 at 100 kHz
[ 0.906988] pca953x 3-0020: 3-0020 supply vcc not found, using dummy regulator
[ 0.935923] pca953x 3-0022: 3-0022 supply vcc not found, using dummy regulator
[ 0.943964] GPIO line 481 (MCASP/TRACE_MUX_S0) hogged as output/low
[ 0.950558] GPIO line 482 (MCASP/TRACE_MUX_S1) hogged as output/high
[ 0.957395] omap_i2c 2000000.i2c: bus 3 rev0.12 at 400 kHz
[ 0.963449] omap_i2c 2010000.i2c: bus 4 rev0.12 at 400 kHz
[ 0.969385] omap_i2c 2020000.i2c: bus 5 rev0.12 at 100 kHz
[ 0.975326] pca953x 6-0020: 6-0020 supply vcc not found, using dummy regulator
[ 1.003720] omap_i2c 2030000.i2c: bus 6 rev0.12 at 400 kHz
[ 1.009645] omap_i2c 2040000.i2c: bus 7 rev0.12 at 100 kHz
[ 1.015512] omap_i2c 2050000.i2c: bus 8 rev0.12 at 100 kHz
[ 1.021455] pca953x 9-0020: 9-0020 supply vcc not found, using dummy regulator
[ 1.051669] omap_i2c 2060000.i2c: bus 9 rev0.12 at 400 kHz
[ 1.057926] ti-sci-intr interconnect@100000:interconnect@28380000:interrupt-controller2: Interrupt Router 137 domain created
[ 1.069495] ti-sci-intr interconnect@100000:interrupt-controller0: Interrupt Router 131 domain created
[ 1.079102] ti-sci-intr interconnect@100000:navss@30000000:interrupt-controller1: Interrupt Router 213 domain created
[ 1.090108] ti-sci-inta 33d00000.interrupt-controller: Interrupt Aggregator domain 209 created
[ 1.107179] cdns-torrent-phy 5050000.serdes: 4 lanes, max bit rate 5.400 Gbps
[ 2.115781] j721e-pcie 2900000.pcie: host bridge /interconnect@100000/pcie@2900000 ranges:
[ 2.124254] j721e-pcie 2900000.pcie: IO 0x10001000..0x10010fff -> 0x10001000
[ 2.131731] j721e-pcie 2900000.pcie: MEM 0x10011000..0x17ffffff -> 0x10011000
[ 2.139301] j721e-pcie 2900000.pcie: PCI host bridge to bus 0000:00
[ 2.145710] pci_bus 0000:00: root bus resource [bus 00-0f]
[ 2.151314] pci_bus 0000:00: root bus resource [io 0x0000-0xffff] (bus address [0x10001000-0x10010fff])
[ 2.161004] pci_bus 0000:00: root bus resource [mem 0x10011000-0x17ffffff]
[ 2.168045] pci 0000:00:00.0: [104c:b00d] type 01 class 0x060400
[ 2.174200] pci_bus 0000:00: 2-byte config write to 0000:00:00.0 offset 0x4 may corrupt adjacent RW1C bits
[ 2.184069] pci_bus 0000:00: 2-byte config write to 0000:00:00.0 offset 0x4 may corrupt adjacent RW1C bits
[ 2.193955] pci_bus 0000:00: 2-byte config write to 0000:00:00.0 offset 0xe8 may corrupt adjacent RW1C bits
[ 2.203913] pci_bus 0000:00: 2-byte config write to 0000:00:00.0 offset 0x3e may corrupt adjacent RW1C bits
[ 2.213880] pci_bus 0000:00: 2-byte config write to 0000:00:00.0 offset 0x92 may corrupt adjacent RW1C bits
[ 2.223842] pci_bus 0000:00: 2-byte config write to 0000:00:00.0 offset 0xb2 may corrupt adjacent RW1C bits
[ 2.233842] pci 0000:00:00.0: supports D1
[ 2.237935] pci 0000:00:00.0: PME# supported from D0 D1 D3hot
[ 2.243807] pci_bus 0000:00: 2-byte config write to 0000:00:00.0 offset 0x84 may corrupt adjacent RW1C bits
[ 2.253772] pci_bus 0000:00: 2-byte config write to 0000:00:00.0 offset 0x208 may corrupt adjacent RW1C bits
[ 2.263824] pci 0000:00:00.0: reg 0x224: [mem 0x00000000-0x003fffff 64bit]
[ 2.270849] pci 0000:00:00.0: VF(n) BAR0 space: [mem 0x00000000-0x00ffffff 64bit] (contains BAR0 for 4 VFs)
[ 2.280816] pci_bus 0000:00: 2-byte config write to 0000:00:00.0 offset 0x210 may corrupt adjacent RW1C bits
[ 2.290863] pci_bus 0000:00: 2-byte config write to 0000:00:00.0 offset 0x210 may corrupt adjacent RW1C bits
[ 2.302549] pci 0000:00:00.0: bridge configuration invalid ([bus 00-00]), reconfiguring
[ 2.312184] pci_bus 0000:01: busn_res: [bus 01-0f] end is updated to 01
[ 2.318955] pci 0000:00:00.0: BAR 7: assigned [mem 0x10400000-0x113fffff 64bit]
[ 2.326431] pci 0000:00:00.0: PCI bridge to [bus 01]
[ 2.331709] pcieport 0000:00:00.0: PME: Signaling with IRQ 40
[ 2.337731] pcieport 0000:00:00.0: AER: enabled with IRQ 40
[ 3.345552] j721e-pcie 2910000.pcie: host bridge /interconnect@100000/pcie@2910000 ranges:
[ 3.354029] j721e-pcie 2910000.pcie: IO 0x18001000..0x18010fff -> 0x18001000
[ 3.361506] j721e-pcie 2910000.pcie: MEM 0x18011000..0x1fffffff -> 0x18011000
[ 3.369038] j721e-pcie 2910000.pcie: PCI host bridge to bus 0001:00
[ 3.375444] pci_bus 0001:00: root bus resource [bus 00-0f]
[ 3.381048] pci_bus 0001:00: root bus resource [io 0x10000-0x1ffff] (bus address [0x18001000-0x18010fff])
[ 3.390916] pci_bus 0001:00: root bus resource [mem 0x18011000-0x1fffffff]
[ 3.397952] pci 0001:00:00.0: [104c:b00d] type 01 class 0x060400
[ 3.404153] pci 0001:00:00.0: supports D1
[ 3.408247] pci 0001:00:00.0: PME# supported from D0 D1 D3hot
[ 3.415667] pci 0001:00:00.0: bridge configuration invalid ([bus 00-00]), reconfiguring
[ 3.425293] pci_bus 0001:01: busn_res: [bus 01-0f] end is updated to 01
[ 3.432059] pci 0001:00:00.0: PCI bridge to [bus 01]
[ 3.437300] pcieport 0001:00:00.0: PME: Signaling with IRQ 43
[ 3.443292] pcieport 0001:00:00.0: AER: enabled with IRQ 43
[ 4.451225] j721e-pcie 2920000.pcie: host bridge /interconnect@100000/pcie@2920000 ranges:
[ 4.459705] j721e-pcie 2920000.pcie: IO 0x4400001000..0x4400010fff -> 0x00001000
[ 4.467537] j721e-pcie 2920000.pcie: MEM 0x4400011000..0x4407ffffff -> 0x00011000
[ 4.475427] j721e-pcie 2920000.pcie: PCI host bridge to bus 0002:00
[ 4.481833] pci_bus 0002:00: root bus resource [bus 00-0f]
[ 4.487437] pci_bus 0002:00: root bus resource [io 0x20000-0x2ffff] (bus address [0x1000-0x10fff])
[ 4.496684] pci_bus 0002:00: root bus resource [mem 0x4400011000-0x4407ffffff] (bus address [0x00011000-0x07ffffff])
[ 4.507451] pci 0002:00:00.0: [104c:b00d] type 01 class 0x060400
[ 4.513653] pci 0002:00:00.0: supports D1
[ 4.517747] pci 0002:00:00.0: PME# supported from D0 D1 D3hot
[ 4.525160] pci 0002:00:00.0: bridge configuration invalid ([bus 00-00]), reconfiguring
[ 4.534793] pci_bus 0002:01: busn_res: [bus 01-0f] end is updated to 01
[ 4.541559] pci 0002:00:00.0: PCI bridge to [bus 01]
[ 4.546794] pcieport 0002:00:00.0: PME: Signaling with IRQ 46
[ 4.552789] pcieport 0002:00:00.0: AER: enabled with IRQ 46
[ 4.559188] k3-ringacc 2b800000.ringacc: Ring Accelerator probed rings:286, gp-rings[96,20] sci-dev-id:235
[ 4.569067] k3-ringacc 2b800000.ringacc: dma-ring-reset-quirk: disabled
[ 4.575827] k3-ringacc 2b800000.ringacc: RA Proxy rev. 66346100, num_proxies:64
[ 4.584678] k3-ringacc 3c000000.ringacc: Ring Accelerator probed rings:1024, gp-rings[440,150] sci-dev-id:211
[ 4.594828] k3-ringacc 3c000000.ringacc: dma-ring-reset-quirk: disabled
[ 4.601587] k3-ringacc 3c000000.ringacc: RA Proxy rev. 66346100, num_proxies:64
[ 4.609292] omap8250 40a00000.serial: PM domain pd:149 will not be powered off
[ 4.616846] 40a00000.serial: ttyS1 at MMIO 0x40a00000 (irq = 7, base_baud = 6000000) is a 8250
[ 4.626025] 2800000.serial: ttyS2 at MMIO 0x2800000 (irq = 19, base_baud = 3000000) is a 8250
[ 4.634770] printk: console [ttyS2] enabled
[ 4.634770] printk: console [ttyS2] enabled
[ 4.643206] printk: bootconsole [ns16550a0] disabled
[ 4.643206] printk: bootconsole [ns16550a0] disabled
[ 4.653563] 2810000.serial: ttyS3 at MMIO 0x2810000 (irq = 20, base_baud = 3000000) is a 8250
[ 4.662406] 2840000.serial: ttyS6 at MMIO 0x2840000 (irq = 21, base_baud = 3000000) is a 8250
[ 4.671160] arm-smmu-v3 36600000.smmu: ias 48-bit, oas 48-bit (features 0x00001faf)
[ 4.680093] arm-smmu-v3 36600000.smmu: allocated 524288 entries for cmdq
[ 4.688980] arm-smmu-v3 36600000.smmu: allocated 524288 entries for evtq
[ 4.696610] arm-smmu-v3 36600000.smmu: msi_domain absent - falling back to wired irqs
[ 4.706451] cdns-ufshcd 4e84000.ufs: ufshcd_populate_vreg: Unable to find vdd-hba-supply regulator, assuming enabled
[ 4.716977] cdns-ufshcd 4e84000.ufs: ufshcd_populate_vreg: Unable to find vcc-supply regulator, assuming enabled
[ 4.727130] cdns-ufshcd 4e84000.ufs: ufshcd_populate_vreg: Unable to find vccq-supply regulator, assuming enabled
[ 4.737368] cdns-ufshcd 4e84000.ufs: ufshcd_populate_vreg: Unable to find vccq2-supply regulator, assuming enabled
[ 4.748162] scsi host0: ufshcd
[ 4.754952] cadence-qspi 47040000.spi: mt35xu512aba (65536 Kbytes)
[ 4.761141] 7 cmdlinepart partitions found on MTD device 47040000.spi.0
[ 4.767738] Creating 7 MTD partitions on "47040000.spi.0":
[ 4.773218] cdns-ufshcd 4e84000.ufs: ufshcd_print_pwr_info:[RX, TX]: gear=[1, 1], lane[1, 1], pwr[SLOWAUTO_MODE, SLOWAUTO_MODE], rate = 0
[ 4.773221] 0x000000000000-0x000000080000 : "ospi.tiboot3"
[ 4.786050] 0x000000080000-0x000000280000 : "ospi.tispl"
[ 4.796777] 0x000000280000-0x000000680000 : "ospi.u-boot"
[ 4.802578] 0x000000680000-0x0000006a0000 : "ospi.env"
[ 4.808133] 0x0000006a0000-0x0000006c0000 : "ospi.env.backup"
[ 4.814277] 0x0000006c0000-0x0000007c0000 : "ospi.sysfw"
[ 4.820003] 0x000000800000-0x000004000000 : "ospi.rootfs"
[ 4.837398] cdns-ufshcd 4e84000.ufs: ufshcd_print_pwr_info:[RX, TX]: gear=[3, 3], lane[2, 2], pwr[FAST MODE, FAST MODE], rate = 2
[ 4.849066] cdns-ufshcd 4e84000.ufs: ufshcd_find_max_sup_active_icc_level: Regulator capability was not set, actvIccLevel=0
[ 4.860356] scsi 0:0:0:49488: Well-known LUN TOSHIBA THGAF8G8T23BAILB 0300 PQ: 0 ANSI: 6
[ 4.869128] scsi 0:0:0:49476: Well-known LUN TOSHIBA THGAF8G8T23BAILB 0300 PQ: 0 ANSI: 6
[ 4.877891] cdns-ufshcd 4e84000.ufs: ufshcd_scsi_add_wlus: BOOT WLUN not found
[ 5.075617] cadence-qspi 47040000.spi: Cadence QSPI NOR probe failed -517
[ 5.083369] cadence-qspi 47050000.spi: mt25qu512a (65536 Kbytes)
[ 5.119583] cadence-qspi 47050000.spi: Cadence QSPI NOR probe failed -517
[ 5.163368] davinci_mdio 46000f00.mdio: davinci mdio revision 9.7, bus freq 1000000
[ 5.171011] libphy: 46000f00.mdio: probed
[ 5.176079] davinci_mdio 46000f00.mdio: phy[0]: device 46000f00.mdio:00, driver TI DP83867
[ 5.184343] am65-cpsw-nuss 46000000.ethernet: initializing am65 cpsw nuss version 0x6BA00101, cpsw version 0x6BA80100 Ports: 2
[ 5.195793] am65-cpsw-nuss 46000000.ethernet: Failed to request tx dma channel -517
[ 5.204510] am65-cpts 310d0000.cpts: CPTS ver 0x4e8a010a, freq:200000000, add_val:4 pps:0
[ 5.213077] mmc0: CQHCI version 5.10
[ 5.251456] mmc0: SDHCI controller on 4f80000.sdhci [4f80000.sdhci] using ADMA 64-bit
[ 5.260210] davinci-mcasp 2ba0000.mcasp: IRQ common not found
[ 5.266784] davinci_gpio 42110000.gpio: IRQ index 4 not found
[ 5.272557] davinci_gpio 42110000.gpio: IRQ not populated, err = -6
[ 5.282741] vdd_mmc1: supplied by vsys_3v3
[ 5.287283] pca953x 4-0020: 4-0020 supply vcc not found, using dummy regulator
[ 5.315901] GPIO line 284 (DP0_PWR_SW_EN) hogged as output/high
[ 5.322501] omap-mailbox 31f80000.mailbox: omap mailbox rev 0x66fc7100
[ 5.329355] omap-mailbox 31f81000.mailbox: omap mailbox rev 0x66fc7100
[ 5.336219] omap-mailbox 31f82000.mailbox: omap mailbox rev 0x66fc7100
[ 5.343070] omap-mailbox 31f83000.mailbox: omap mailbox rev 0x66fc7100
[ 5.349931] omap-mailbox 31f84000.mailbox: omap mailbox rev 0x66fc7100
[ 5.359643] ti-udma 285c0000.dma-controller: Channels: 24 (tchan: 12, rchan: 12, gp-rflow: 8)
[ 5.370095] ti-udma 31150000.dma-controller: Channels: 84 (tchan: 42, rchan: 42, gp-rflow: 16)
[ 5.383355] cadence-qspi 47040000.spi: mt35xu512aba (65536 Kbytes)
[ 5.389598] 7 cmdlinepart partitions found on MTD device 47040000.spi.0
[ 5.396287] Creating 7 MTD partitions on "47040000.spi.0":
[ 5.401800] 0x000000000000-0x000000080000 : "ospi.tiboot3"
[ 5.407831] 0x000000080000-0x000000280000 : "ospi.tispl"
[ 5.413542] 0x000000280000-0x000000680000 : "ospi.u-boot"
[ 5.419506] mmc0: Command Queue Engine enabled
[ 5.423946] mmc0: new HS400 MMC card at address 0001
[ 5.428931] 0x000000680000-0x0000006a0000 : "ospi.env"
[ 5.434493] mmcblk0: mmc0:0001 S0J56X 14.8 GiB
[ 5.439152] mmcblk0boot0: mmc0:0001 S0J56X partition 1 31.5 MiB
[ 5.445402] 0x0000006a0000-0x0000006c0000 : "ospi.env.backup"
[ 5.451297] mmcblk0boot1: mmc0:0001 S0J56X partition 2 31.5 MiB
[ 5.457578] 0x0000006c0000-0x0000007c0000 : "ospi.sysfw"
[ 5.462910] mmcblk0rpmb: mmc0:0001 S0J56X partition 3 4.00 MiB, chardev (240:0)
[ 5.470604] 0x000000800000-0x000004000000 : "ospi.rootfs"
[ 5.478907] cadence-qspi 47050000.spi: mt25qu512a (65536 Kbytes)
[ 5.484968] mmcblk0: p1 p2
[ 5.527366] davinci_mdio 46000f00.mdio: davinci mdio revision 9.7, bus freq 1000000
[ 5.535014] libphy: 46000f00.mdio: probed
[ 5.540074] davinci_mdio 46000f00.mdio: phy[0]: device 46000f00.mdio:00, driver TI DP83867
[ 5.548338] am65-cpsw-nuss 46000000.ethernet: initializing am65 cpsw nuss version 0x6BA00101, cpsw version 0x6BA80100 Ports: 2
[ 5.560500] am65-cpsw-nuss 46000000.ethernet: set new flow-id-base 48
[ 5.567650] pps pps0: new PPS source ptp1
[ 5.571764] am65-cpsw-nuss 46000000.ethernet: CPTS ver 0x4e8a010a, freq:500000000, add_val:1 pps:1
[ 5.580716] am65-cpsw-nuss 46000000.ethernet: initialized cpsw ale version 57.4
[ 5.588009] am65-cpsw-nuss 46000000.ethernet: ALE Table size 64
[ 5.595029] mmc1: CQHCI version 5.10
[ 5.629463] mmc1: SDHCI controller on 4fb0000.sdhci [4fb0000.sdhci] using ADMA 64-bit
[ 5.637629] davinci-mcasp 2ba0000.mcasp: IRQ common not found
[ 5.649712] debugfs: Directory 'pd:242' with parent 'pm_genpd' already present!
[ 5.657129] debugfs: Directory 'pd:241' with parent 'pm_genpd' already present!
[ 5.664494] debugfs: Directory 'pd:240' with parent 'pm_genpd' already present!
[ 5.671811] debugfs: Directory 'pd:239' with parent 'pm_genpd' already present!
[ 5.679901] hctosys: unable to open rtc device (rtc0)
[ 5.700111] ALSA device list:
[ 5.703065] No soundcards found.
[ 5.725592] EXT4-fs (mmcblk0p2): recovery complete
[ 5.730949] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
[ 5.739066] VFS: Mounted root (ext4 filesystem) on device 179:2.
[ 5.746294] devtmpfs: mounted
[ 5.749645] Freeing unused kernel memory: 1728K
[ 5.754196] Run /sbin/init as init process
[ 5.807185] systemd[1]: System time before build time, advancing clock.
[ 5.833127] NET: Registered protocol family 10
[ 5.838002] Segment Routing with IPv6
[ 5.849768] systemd[1]: systemd 244.3+ running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR -SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN2 -IDN -PCRE2 default-hierarchy=hybrid)
[ 5.871520] systemd[1]: Detected architecture arm64.
Welcome to Arago 2020.05!
[ 5.911709] systemd[1]: Set hostname to <j7-evm>.
[ 6.048303] systemd[1]: /lib/systemd/system/docker.socket:6: ListenStream= references a path below legacy directory /var/run/, updating /var/run/docker.sock �� /run/docker.sock; please update the unit file accordingly.
[ 6.103693] random: systemd: uninitialized urandom read (16 bytes read)
[ 6.110405] systemd[1]: system-getty.slice: unit configures an IP firewall, but the local system does not support BPF/cgroup firewalling.
[ 6.122730] systemd[1]: (This warning is only shown for the first unit using IP firewalling.)
[ 6.132619] systemd[1]: Created slice system-getty.slice.
[ OK ] Created slice system-getty.slice.
[ 6.155448] random: systemd: uninitialized urandom read (16 bytes read)
[ 6.162683] systemd[1]: Created slice system-serial\x2dgetty.slice.
[ OK ] Created slice system-serial\x2dgetty.slice.
[ 6.183428] random: systemd: uninitialized urandom read (16 bytes read)
[ 6.190555] systemd[1]: Created slice User and Session Slice.
[ OK ] Created slice User and Session Slice.
[ 6.211544] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
[ OK ] Started Dispatch Password ��ts to Console Directory Watch.
[ 6.235471] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[ OK ] Started Forward Password R��uests to Wall Directory Watch.
[ 6.259466] systemd[1]: Reached target Paths.
[ OK ] Reached target Paths.
[ 6.275418] systemd[1]: Reached target Remote File Systems.
[ OK ] Reached target Remote File Systems.
[ 6.295407] systemd[1]: Reached target Slices.
[ OK ] Reached target Slices.
[ 6.311410] systemd[1]: Reached target Swap.
[ OK ] Reached target Swap.
[ 6.330358] systemd[1]: Listening on RPCbind Server Activation Socket.
[ OK ] Listening on RPCbind Server Activation Socket.
[ 6.351442] systemd[1]: Reached target RPC Port Mapper.
[ OK ] Reached target RPC Port Mapper.
[ 6.373336] systemd[1]: Listening on Process Core Dump Socket.
[ OK ] Listening on Process Core Dump Socket.
[ 6.395597] systemd[1]: Listening on initctl Compatibility Named Pipe.
[ OK ] Listening on initctl Compatibility Named Pipe.
[ 6.419227] systemd[1]: Condition check resulted in Journal Audit Socket being skipped.
[ 6.427581] systemd[1]: Listening on Journal Socket (/dev/log).
[ OK ] Listening on Journal Socket (/dev/log).
[ 6.447650] systemd[1]: Listening on Journal Socket.
[ OK ] Listening on Journal Socket.
[ 6.463693] systemd[1]: Listening on Network Service Netlink Socket.
[ OK ] Listening on Network Service Netlink Socket.
[ 6.487593] systemd[1]: Listening on udev Control Socket.
[ OK ] Listening on udev Control Socket.
[ 6.507521] systemd[1]: Listening on udev Kernel Socket.
[ OK ] Listening on udev Kernel Socket.
[ 6.531815] systemd[1]: Mounting Huge Pages File System...
Mounting Huge Pages File System...
[ 6.550803] systemd[1]: Mounting POSIX Message Queue File System...
Mounting POSIX Message Queue File System...
[ 6.575596] systemd[1]: Mounting Kernel Debug File System...
Mounting Kernel Debug File System...
[ 6.601156] systemd[1]: Mounting Temporary Directory (/tmp)...
Mounting Temporary Directory (/tmp)...
[ 6.620484] systemd[1]: Starting Create list of static device nodes for the current kernel...
Starting Create list of st��odes for the current kernel...
[ 6.647017] systemd[1]: Starting Start psplash boot splash screen...
Starting Start psplash boot splash screen...
[ 6.676953] systemd[1]: Started Hardware RNG Entropy Gatherer Daemon.
[ OK ] Started Hardware RNG Entropy Gatherer Daemon.
[ 6.698877] systemd[1]: Starting RPC Bind...
Starting RPC Bind...
[ 6.715591] systemd[1]: Condition check resulted in File System Check on Root Device being skipped.
[ 6.735916] systemd[1]: Starting Journal Service...
Starting Journal Service...
[ 6.761547] systemd[1]: Starting Load Kernel Modules...
Starting Load Kernel Modules...
[ 6.782048] cryptodev: loading out-of-tree module taints kernel.
[ 6.792244] systemd[1]: Starting Remount Root and Kernel File Systems...
Starting Remount Root and Kernel File Systems...
[ 6.810167] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)
[ 6.820379] systemd[1]: Starting udev Coldplug all Devices...
[ 6.831602] cryptodev: driver 1.10 loaded.
Starting udev Coldplug all Devices...
[ 6.844514] systemd[1]: Started RPC Bind.
[ OK ] Started RPC Bind.
[ 6.864735] systemd[1]: Started Journal Service.
[ OK ] Started Journal Service.
[ OK ] Mounted Huge Pages File System.
[ OK ] Mounted POSIX Message Queue File System.
[ OK ] Mounted Kernel Debug File System.
[ OK ] Mounted Temporary Directory (/tmp).
[ OK ] Started Create list of sta�� nodes for the current kernel.
[FAILED] Failed to start Start psplash boot splash screen.
See 'systemctl status psplash-start.service' for details.
[DEPEND] Dependency failed for Star��progress communication helper.
[ OK ] Started Load Kernel Modules.
[ OK ] Started Remount Root and Kernel File Systems.
Mounting Kernel Configuration File System...
Starting Flush Journal to Persistent Storage...
[ 7.079902] systemd-journald[229]: Received client request to flush runtime journal.
Starting Apply Kernel Variables...
Starting Create Static Device Nodes in /dev...
[ OK ] Mounted Kernel Configuration File System.
[ OK ] Started Flush Journal to Persistent Storage.
[ OK ] Started Apply Kernel Variables.
[ OK ] Started Create Static Device Nodes in /dev.
[ OK ] Reached target Local File Systems (Pre).
Mounting /media/ram...
Mounting /var/volatile...
Starting udev Kernel Device Manager...
[ OK ] Started udev Coldplug all Devices.
[ OK ] Mounted /media/ram.
[ OK ] Started udev Kernel Device Manager.
[ OK ] Mounted /var/volatile.
Starting Load/Save Random Seed...
[ OK ] Reached target Local File Systems.
Starting Create Volatile Files and Directories...
[ OK ] Started Create Volatile Files and Directories.
Starting Network Time Synchronization...
Starting Update UTMP about System Boot/Shutdown...
[ OK ] Started Update UTMP about System Boot/Shutdown.
[ OK ] Started Network Time Synchronization.
[ OK ] Reached target System Initialization.
[ OK ] Started Daily Cleanup of Temporary Directories.
[ OK ] Reached target System Time Set.
[ OK ] Reached target System Time Synchronized.
[ OK ] Started Daily rotation of log files.
[ OK ] Reached target Timers.
[ OK ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
[ OK ] Listening on D-Bus System Message Bus Socket.
Starting Docker Socket for the API.
[ OK ] Listening on dropbear.socket.
Starting Reboot and dump vmcore via kexec...
[ OK ] Listening on Docker Socket for the API.
[ OK ] Reached target Sockets.
[ OK ] Reached target Basic System.
[ OK ] Started Job spooling tools.
[ OK ] Started Periodic Command Scheduler.
[ OK ] Started D-Bus System Message Bus.
Starting Print notice about GPLv3 packages...
Starting IPv6 Packet Filtering Framework...
Starting IPv4 Packet Filtering Framework...
[ OK ] Started irqbalance daemon.
Starting rc.pvr.service...
Starting Login Service...
[ OK ] Started TEE Supplicant.
[ OK ] Started Reboot and dump vmcore via kexec.
[ OK ] Started IPv6 Packet Filtering Framework.
[ OK ] Started IPv4 Packet Filtering Framework.
[ OK ] Reached target Network (Pre).
Starting Network Service...
[ OK ] Started Network Service.
Starting Wait for Network to be Configured...
Starting Network Name Resolution...
[ 8.059892] PVR_K: 310: Read BVNC 22.104.208.318 from HW device registers
[ 8.068965] PVR_K: 310: RGX Device initialised with BVNC 22.104.208.318
[ 8.097475] [drm] Initialized pvr 1.10.5371573 20170530 for 4e20000000.gpu on minor 0
[ 8.113201] rti-wdt 2200000.rti: heartbeat 60 sec
[ OK ] Started Login Service.
[ OK ] Started Network Name Resolution.
[ OK ] Reached target Network.
[ OK ] Reached target Host and Network Name Lookups.
Starting Avahi mDNS/DNS-SD Stack...
[ OK ] Started NFS status monitor for NFSv2/3 locking..
Starting Permit User Sessions...
[ OK ] Started Avahi mDNS/DNS-SD Stack.
[ 8.259825] rti-wdt 2210000.rti: heartbeat 60 sec
[ OK ] Started Permit User Sessions.
[ OK ] Started Getty on tty1.
[ OK ] Started Serial Getty on ttyS2.
[ OK ] Started Serial Getty on ttyS3.
[ OK ] Reached target Login Prompts.
Starting Synchronize System and HW clocks...
[FAILED] Failed to start Synchronize System and HW clocks.
See 'systemctl status sync-clocks.service' for details.
[ 8.958755] k3-dsp-rproc 4d80800000.dsp: assigned reserved memory node c66-dma-memory@a7000000
[ 9.176958] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[ 9.186653] [drm] No driver support for vblank timestamp query.
[ 9.196184] [drm] Initialized tidss 1.0.0 20180215 for 4a00000.dss on minor 1
[ 9.208510] [drm] Cannot find any crtc or sizes
[ 9.395865] k3-dsp-rproc 4d80800000.dsp: configured DSP for remoteproc mode
***************************************************************
***************************************************************
NOTICE: This file system contains the following GPLv3 packages:
bash-dev
bash
bc
binutils
cifs-utils
cpio
dosfstools
elfutils
gawk
gdb
gdbserver
glmark2
gstreamer1.[ 9.595413] random: crng init done
0-libav
gzip
less
libasm1
libbfd
libdw1
libelf1
li[ 9.600289] random: 7 urandom warning(s) missed due to ratelimiting
bgdbm-compat4
libgdbm-dev
libgdbm6
libgmp10
libidn2-0
libreadline-dev
libreadline8
libunistring2
m4-dev
m4
nettle
parted
tar
which
If you do not wish to distribute[ 9.628241] remoteproc remoteproc0: 4d80800000.dsp is available
GPLv3 components please remove
the above packages prior to distribution. This can be done using
the opkg remove command. i.e.:
opkg remove <package>
Where <package> is the name printed in the list above
NOTE: If the package is a dependency of another package you
will be notified of the dependent packages. You should
use the --force-removal-of-dependent-packages option to
also remove the dependent packages as well
***************************************************************
***************************************************************
[ OK ] Started Load/Save Random Seed.
[ OK ] Started Print notice about GPLv3 packages.
[ 9.827977] remoteproc remoteproc0: Direct firmware load for j7-c66_0-fw failed with error -2
[ 9.838512] k3-dsp-rproc 4d81800000.dsp: assigned reserved memory node c66-dma-memory@a6000000
[ 9.847201] remoteproc remoteproc0: powering up 4d80800000.dsp
[ 9.853091] remoteproc remoteproc0: Direct firmware load for j7-c66_0-fw failed with error -2
[ 9.861729] remoteproc remoteproc0: request_firmware failed: -2
[ 9.899637] k3-dsp-rproc 4d81800000.dsp: configured DSP for remoteproc mode
[ 9.932248] platform 41000000.r5f: configured R5F for IPC-only mode
[ 10.011837] platform 41000000.r5f: assigned reserved memory node r5f-dma-memory@a0000000
[ 10.122435] remoteproc remoteproc1: 4d81800000.dsp is available
[ 10.211553] remoteproc remoteproc2: 41000000.r5f is available
[ 10.251525] remoteproc remoteproc1: Direct firmware load for j7-c66_1-fw failed with error -2
[ 10.263481] remoteproc remoteproc1: powering up 4d81800000.dsp
[ 10.269338] remoteproc remoteproc1: Direct firmware load for j7-c66_1-fw failed with error -2
[ 10.283474] k3-dsp-rproc 64800000.dsp: assigned reserved memory node c71-dma-memory@a8000000
[ 10.291941] remoteproc remoteproc1: request_firmware failed: -2
[ 10.352523] remoteproc remoteproc2: powering up 41000000.r5f
[ 10.358226] remoteproc remoteproc2: Booting fw image j7-mcu-r5f0_0-fw, size 190412
[ 10.371542] platform 41000000.r5f: R5F core initialized in IPC-only mode
[ 10.380093] platform 5c00000.r5f: configured R5F for IPC-only mode
[ 10.386307] remoteproc2#vdev0buffer: assigned reserved memory node r5f-dma-memory@a0000000
[ 10.395235] virtio_rpmsg_bus virtio0: rpmsg host is online
[ 10.407465] remoteproc2#vdev0buffer: registered virtio0 (type 7)
[ 10.413791] remoteproc remoteproc2: remote processor 41000000.r5f is now up
[ 10.420804] virtio_rpmsg_bus virtio0: creating channel rpmsg_chrdev addr 0xd
[ 10.490508] k3-dsp-rproc 64800000.dsp: configured DSP for IPC-only mode
[ 10.504196] platform 5c00000.r5f: assigned reserved memory node r5f-dma-memory@a1000000
[ 10.568822] TI DP83867 46000f00.mdio:00: attached PHY driver [TI DP83867] (mii_bus:phy_addr=46000f00.mdio:00, irq=POLL)
[ 10.590693] am65-cpsw-nuss 46000000.ethernet eth0: Link is Down
[ 10.643794] remoteproc remoteproc3: 64800000.dsp is available
[ 10.687538] remoteproc remoteproc4: 5c00000.r5f is available
[ 10.772922] remoteproc remoteproc3: powering up 64800000.dsp
[ 10.778633] remoteproc remoteproc3: Booting fw image j7-c71_0-fw, size 6590448
[ 10.791524] k3-dsp-rproc 64800000.dsp: DSP initialized in IPC-only mode
[ 10.802362] remoteproc3#vdev0buffer: assigned reserved memory node c71-dma-memory@a8000000
[ 10.815904] virtio_rpmsg_bus virtio1: rpmsg host is online
[ 10.821476] remoteproc3#vdev0buffer: registered virtio1 (type 7)
[ 10.831393] remoteproc remoteproc3: remote processor 64800000.dsp is now up
[ 10.838442] virtio_rpmsg_bus virtio1: creating channel rpmsg_chrdev addr 0xd
[ 10.899274] remoteproc remoteproc4: powering up 5c00000.r5f
[ 10.904879] remoteproc remoteproc4: Booting fw image j7-main-r5f0_0-fw, size 215396
[ 10.916554] platform 5c00000.r5f: R5F core initialized in IPC-only mode
[ 10.923181] remoteproc4#vdev0buffer: assigned reserved memory node r5f-dma-memory@a1000000
[ 10.939760] virtio_rpmsg_bus virtio2: rpmsg host is online
[ 10.945259] remoteproc4#vdev0buffer: registered virtio2 (type 7)
[ 10.945972] virtio_rpmsg_bus virtio2: creating channel rpmsg_chrdev addr 0xd
[ 10.956970] remoteproc remoteproc4: remote processor 5c00000.r5f is now up
[ 10.965578] platform 5d00000.r5f: configured R5F for IPC-only mode
[ 11.095806] platform 5d00000.r5f: assigned reserved memory node r5f-dma-memory@a3000000
[ 11.148384] remoteproc remoteproc5: 5d00000.r5f is available
[ 11.204276] remoteproc remoteproc5: powering up 5d00000.r5f
[ 11.209924] remoteproc remoteproc5: Booting fw image j7-main-r5f0_1-fw, size 141164
[ 11.217735] platform 5d00000.r5f: R5F core initialized in IPC-only mode
[ 11.232860] remoteproc5#vdev0buffer: assigned reserved memory node r5f-dma-memory@a3000000
[ 11.251852] virtio_rpmsg_bus virtio3: rpmsg host is online
[ 11.257923] platform 5e00000.r5f: configured R5F for IPC-only mode
[ 11.261057] remoteproc5#vdev0buffer: registered virtio3 (type 7)
[ 11.264151] virtio_rpmsg_bus virtio3: creating channel rpmsg_chrdev addr 0xd
[ 11.275363] remoteproc remoteproc5: remote processor 5d00000.r5f is now up
[ 11.467465] platform 5e00000.r5f: assigned reserved memory node r5f-dma-memory@a4000000
[ 11.545350] j721e-audio sound@0: pcm3168a-dac <-> 2ba0000.mcasp mapping ok
[ 11.606009] remoteproc remoteproc6: 5e00000.r5f is available
[ 11.623589] j721e-audio sound@0: pcm3168a-adc <-> 2ba0000.mcasp mapping ok
[ 11.678798] remoteproc remoteproc6: powering up 5e00000.r5f
[ 11.684447] remoteproc remoteproc6: Booting fw image j7-main-r5f1_0-fw, size 141164
[ 11.695507] platform 5e00000.r5f: R5F core initialized in IPC-only mode
[ 11.703395] platform 5f00000.r5f: configured R5F for IPC-only mode
[ 11.709614] remoteproc6#vdev0buffer: assigned reserved memory node r5f-dma-memory@a4000000
[ 11.718361] virtio_rpmsg_bus virtio4: rpmsg host is online
[ 11.725130] virtio_rpmsg_bus virtio4: creating channel rpmsg_chrdev addr 0xd
[ 11.727420] remoteproc6#vdev0buffer: registered virtio4 (type 7)
[ 11.743386] remoteproc remoteproc6: remote processor 5e00000.r5f is now up
[ 11.839453] platform 5f00000.r5f: assigned reserved memory node r5f-dma-memory@a5000000
[ 11.997468] remoteproc remoteproc7: 5f00000.r5f is available
[ 12.141889] remoteproc remoteproc7: powering up 5f00000.r5f
[ 12.147595] remoteproc remoteproc7: Booting fw image j7-main-r5f1_1-fw, size 141164
[ 12.162095] platform 5f00000.r5f: R5F core initialized in IPC-only mode
[ 12.168762] remoteproc7#vdev0buffer: assigned reserved memory node r5f-dma-memory@a5000000
[ 12.183827] virtio_rpmsg_bus virtio5: rpmsg host is online
[ 12.193184] remoteproc7#vdev0buffer: registered virtio5 (type 7)
[ 12.203381] remoteproc remoteproc7: remote processor 5f00000.r5f is now up
[ 12.215877] virtio_rpmsg_bus virtio5: creating channel rpmsg_chrdev addr 0xd
[ 12.223085] virtio_rpmsg_bus virtio5: creating channel rpmsg_chrdev addr 0x15
[ 12.235486] virtio_rpmsg_bus virtio1: creating channel rpmsg_chrdev addr 0x15
[ 12.242833] virtio_rpmsg_bus virtio4: creating channel rpmsg_chrdev addr 0x15
[ 12.259513] virtio_rpmsg_bus virtio0: creating channel rpmsg_chrdev addr 0x15
[ 12.266849] virtio_rpmsg_bus virtio2: creating channel rpmsg_chrdev addr 0x15
[ 12.279098] virtio_rpmsg_bus virtio3: creating channel rpmsg_chrdev addr 0x15
[ OK ] Created slice system-weston.slice.
[ OK ] Started Weston Wayland Compositor.
[ OK ] Created slice system-systemd\x2dfsck.slice.
[ OK ] Created slice User Slice of UID 0.
Starting User Runtime Directory /run/user/0...
[ 12.576018] remoteproc remoteproc8: b034000.pru is available
[ OK ] Started User Runtime Directory /run/user/0.
Starting User Manager for UID 0...
[ 12.667436] pru-rproc b034000.pru: PRU rproc node /interconnect@100000/icssg@b000000/pru@34000 probed successfully
[ 12.803646] remoteproc remoteproc9: b004000.rtu is available
[ 12.815511] pru-rproc b004000.rtu: PRU rproc node /interconnect@100000/icssg@b000000/rtu@4000 probed successfully
[ 12.838343] pru-rproc b00a000.txpru: IRQ vring not found
[ 12.852777] pru-rproc b00a000.txpru: IRQ kick not found
[ 12.918831] omap_rng 4e10000.trng: Random Number Generator ver. 241b34c
[ OK ] Started User Manager for UID 0.[ 12.941930] remoteproc remoteproc10: b00a000.txpru is available
[ OK ] Started Session c1 of user root[ 12.969497] pru-rproc b00a000.txpru: PRU rproc node /interconnect@100000/icssg@b000000/txpru@a000 probed successfully
.
[ OK ] Started rc.pvr.service.
Starting weston.service...
[ 13.114172] remoteproc remoteproc11: b038000.pru is available
[ 13.132166] pru-rproc b038000.pru: PRU rproc node /interconnect@100000/icssg@b000000/pru@38000 probed successfully
[ OK ] Found device /dev/mmcblk0p1.
[ 13.237443] remoteproc remoteproc12: b006000.rtu is available
Starting File System Check on /dev/mmcblk0p1...
[ 13.272048] pru-rproc b006000.rtu: PRU rproc node /interconnect@100000/icssg@b000000/rtu@6000 probed successfully
[ 13.306387] cdns-usb3 6000000.usb: DRD version v1 (ID: 0004024e, rev: 00000200)
[ 13.352597] pru-rproc b00c000.txpru: IRQ vring not found
[ 13.368165] pru-rproc b00c000.txpru: IRQ kick not found
[ 13.432005] cdns-usb3 6400000.usb: DRD version v1 (ID: 0004024e, rev: 00000200)
[ 13.436701] remoteproc remoteproc13: b00c000.txpru is available
[ 13.465874] pru-rproc b00c000.txpru: PRU rproc node /interconnect@100000/icssg@b000000/txpru@c000 probed successfully
[ 13.495621] remoteproc remoteproc14: b134000.pru is available
[ 13.565555] pru-rproc b134000.pru: PRU rproc node /interconnect@100000/icssg@b100000/pru@34000 probed successfully
[ 13.622655] remoteproc remoteproc15: b104000.rtu is available
[ 13.629290] usbcore: registered new interface driver usbfs
[ 13.642401] usbcore: registered new interface driver hub
[ 13.644000] pru-rproc b104000.rtu: PRU rproc node /interconnect@100000/icssg@b100000/rtu@4000 probed successfully
[ 13.655997] usbcore: registered new device driver usb
[ 13.703695] pru-rproc b10a000.txpru: IRQ vring not found
[ 13.710730] xhci-hcd xhci-hcd.2.auto: xHCI Host Controller
[ 13.712207] pru-rproc b10a000.txpru: IRQ kick not found
[ 13.723485] xhci-hcd xhci-hcd.2.auto: new USB bus registered, assigned bus number 1
[ 13.731226] remoteproc remoteproc16: b10a000.txpru is available
[ 13.743398] pru-rproc b10a000.txpru: PRU rproc node /interconnect@100000/icssg@b100000/txpru@a000 probed successfully
[ 13.747620] xhci-hcd xhci-hcd.2.auto: hcc params 0x200073c9 hci version 0x100 quirks 0x0000000000010010
[ 13.764109] remoteproc remoteproc17: b138000.pru is available
[ 13.775408] pru-rproc b138000.pru: PRU rproc node /interconnect@100000/icssg@b100000/pru@38000 probed successfully
[ 13.779598] xhci-hcd xhci-hcd.2.auto: irq 516, io mem 0x06410000
[ 13.799928] remoteproc remoteproc18: b106000.rtu is available
[ 13.803722] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 5.04
[ 13.811388] pru-rproc b106000.rtu: PRU rproc node /interconnect@100000/icssg@b100000/rtu@6000 probed successfully
[ 13.823362] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 13.835846] pru-rproc b10c000.txpru: IRQ vring not found
[ 13.839534] usb usb1: Product: xHCI Host Controller
[ 13.847370] pru-rproc b10c000.txpru: IRQ kick not found
[ 13.852821] usb usb1: Manufacturer: Linux 5.4.40-g66cf445b76 xhci-hcd
[ 13.859308] remoteproc remoteproc19: b10c000.txpru is available
[ 13.865337] usb usb1: SerialNumber: xhci-hcd.2.auto
[ 13.870267] pru-rproc b10c000.txpru: PRU rproc node /interconnect@100000/icssg@b100000/txpru@c000 probed successfully
[ 13.875973] hub 1-0:1.0: USB hub found
[ 13.891390] hub 1-0:1.0: 1 port detected
[ 13.904149] xhci-hcd xhci-hcd.2.auto: xHCI Host Controller
[ 13.960131] xhci-hcd xhci-hcd.2.auto: new USB bus registered, assigned bus number 2
[ 14.008070] xhci-hcd xhci-hcd.2.auto: Host supports USB 3.0 SuperSpeed
[ 14.031430] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM.
[ 14.043754] usb usb2: New USB device found, idVendor=1d6b, idProduct=0003, bcdDevice= 5.04
[ 14.061233] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 14.076098] usb usb2: Product: xHCI Host Controller
[ 14.081002] usb usb2: Manufacturer: Linux 5.4.40-g66cf445b76 xhci-hcd
[ 14.095376] usb usb2: SerialNumber: xhci-hcd.2.auto
[ 14.107619] hub 2-0:1.0: USB hub found
[ 14.111393] hub 2-0:1.0: 1 port detected
[ 14.239373] usb 1-1: new high-speed USB device number 2 using xhci-hcd
_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|
Arago Project http://arago-project.org j7-evm ttyS2
Arago 2020.05 j7-evm ttyS2
j7-evm login: [ 14.395639] usb 1-1: New USB device found, idVendor=0451, idProduct=8142, bcdDevice= 1.00
[ 14.407361] usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=1
[ 14.419363] usb 1-1: SerialNumber: D0000859DE36
[ 14.424363] hub 1-1:1.0: USB hub found
[ 14.431379] hub 1-1:1.0: 4 ports detected
j7-evm login: root
Last login: Wed Jun 17 14:43:27 UTC 2020
root@j7-evm:~# cd ..
root@j7-evm:/home# cd ..
root@j7-evm:/# ls
bin dev home init linuxrc media mnt proc sbin tmp var
boot etc include lib lost+found mksdboot.sh opt run sys usr
root@j7-evm:/# cd [ 35.895382] vdd_mmc1: disabling
root@j7-evm:~# cd opt
-sh: cd: opt: No such file or directory
root@j7-evm:~# ls
root@j7-evm:~# pwd
/home/root
root@j7-evm:~# cd ..
root@j7-evm:/home# cd ..
root@j7-evm:/# ls
bin dev home init linuxrc media mnt proc sbin tmp var
boot etc include lib lost+found mksdboot.sh opt run sys usr
root@j7-evm:/# cd opt
root@j7-evm:/opt# ls
containerd img-powervr-sdk ltp vision_apps
root@j7-evm:/opt# cd vision_apps
root@j7-evm:/opt/vision_apps# [ 128.388232] Initializing XFRM netlink socket
[ 128.896340] bridge: filtering via arp/ip/ip6tables is no longer available by default. Update your scripts to load br_netfilter if you need this.
[ 128.910674] Bridge firewalling registered
root@j7-evm:/opt/vision_apps# source ./vision_apps_init.sh
root@j7-evm:/opt/vision_apps# APP_LOG: ERROR: Unable to map memory @ 0xac000000 of size 262144 bytes !!!
root@j7-evm:/opt/vision_apps# ./run_app_tidl.sh
APP: Init ... !!!
APP_LOG: ERROR: Unable to map memory @ 0xac000000 of size 262144 bytes !!!
APP: ERROR: Log writer init failed !!!
APP: Init ... Done !!!
root@j7-evm:/opt/vision_apps#