This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-DRA8X-TDA4X: SDK7.0 linux no response to start

Part Number: PROCESSOR-SDK-DRA8X-TDA4X

We have a problem, which is often unresponsive during startup.Even if you use JTAG, you can't connect.

Condition:

1 MCU2_ 0/mcu2_ 1/MCU3_ 0/MCU3_ 1/C66_ 0/C66_ 1 / C71 firmware is present.

2 psdk: 7.0 ; linux: linux-5.4.40+gitAUTOINC+66cf445b76-g66cf445b76 

3 board: EVM

Possibility 1:

NOTE: If the package is a dependency of another package you
will be notified of the dependent packages. You should
use the --force-removal-of-dependent-packages option to
also remove the dependent packages as well
***************************************************************
***************************************************************
[ OK ] Started Print notice about GPLv3 packages.
[ 16.630697] ti_sci_inta_alloc_irq 2: domain->name=:interconnect@100000:navss@30000000:interrupt-controller@33d00000, hwirq=13828540
[ 16.664007] platform 5e00000.r5f: assigned reserved memory node r5f-dma-memory@a4000000
[ 16.727755] remoteproc remoteproc5: powering up 5d00000.r5f
[ 16.733372] remoteproc remoteproc5: Booting fw image j7-main-r5f0_1-fw, size 5546248
[ 16.745234] remoteproc remoteproc4: powering up 5c00000.r5f
[ 16.750841] remoteproc remoteproc4: Booting fw image j7-main-r5f0_0-fw, size 15211064

Possibility 2:

[ 15.450658] remoteproc remoteproc2: powering up 41000000.r5f
[ OK ] [ 15.459363] remoteproc remoteproc2: Booting fw image j7-mcu-r5f0_0-fw, size 95552
Started Load/Save Random Seed.
[ 15.474840] platform 41000000.r5f: R5F core initialized in IPC-only mode
[ 15.485321] remoteproc2#vdev0buffer: assigned reserved memory node r5f-dma-memory@a0000000
[ 15.500474] virtio_rpmsg_bus virtio1: rpmsg host is online
[ 15.509001] remoteproc2#vdev0buffer: registered virtio1 (type 7)
[ 15.514553] gic_irq_domain_alloc[0] virq + i=522, hwirq + i=296
[ 15.518213] remoteproc remoteproc2: remote processor 41000000.r5f is now up
[ 15.542706] remoteproc remoteproc1: powering up 4d81800000.dsp
[ 15.549745] remoteproc remoteproc1: Booting fw image j7-c66_1-fw, size 10857936
[ 15.561400] k3-dsp-rproc 4d81800000.dsp: DSP initialized in IPC-only mode
[ 15.572596] remoteproc1#vdev0buffer: assigned reserved memory node c66-dma-memory@a6000000
[ 15.580991] k3-ringacc 3c000000.ringacc: dump occ00000000
[ 15.585706] virtio_rpmsg_bus virtio2: rpmsg host is online
[ 15.591184] virtio_rpmsg_bus virtio2: creating channel rpmsg_chrdev addr 0xd
[ 15.594909] remoteproc1#vdev0buffer: registered virtio2 (type 7)
[ 15.609309] remoteproc remoteproc1: remote processor 4d81800000.dsp is now up
[ 15.651179] platform 5c00000.r5f: assigned reserved memory node r5f-dma-memory@a1000000
[ 15.655127] gic_irq_domain_alloc[0] virq + i=523, hwirq + i=297
[ 15.688524] k3-ringacc 3c000000.ringacc: dump indx00000000
[ 15.728689] remoteproc remoteproc4: 5c00000.r5f is available
[ 15.763062] platform 5d00000.r5f: configured R5F for remoteproc mode
[ 15.764656] k3-ringacc 3c000000.ringacc: dump hwocc00000000
[ 15.795442] platform 5d00000.r5f: assigned reserved memory node r5f-dma-memory@a3000000
[ 15.827670] gic_irq_domain_alloc[0] virq + i=524, hwirq + i=298
[ 15.961457] remoteproc remoteproc5: 5d00000.r5f is available
[ 15.992556] gic_irq_domain_alloc[0] virq + i=525, hwirq + i=299
[ 15.998651] remoteproc remoteproc3: powering up 64800000.dsp
[ 16.004362] remoteproc remoteproc3: Booting fw image j7-c71_0-fw, size 15851272
[ 16.011766] k3-dsp-rproc 64800000.dsp: DSP initialized in IPC-only mode
[ 16.022299] remoteproc3#vdev0buffer: assigned reserved memory node c71-dma-memory@a8000000
[ 16.036409] virtio_rpmsg_bus virtio3: rpmsg host is online
[ 16.039279] virtio_rpmsg_bus virtio3: creating channel rpmsg_chrdev addr 0xd
[ 16.041952] remoteproc3#vdev0buffer: registered virtio3 (type 7)
[ 16.065314] remoteproc remoteproc3: remote processor 64800000.dsp is now up
[ 16.078732] k3-ringacc 3c000000.ringacc: dump hwindx00000000
[ 16.108349] gic_irq_domain_alloc[0] virq + i=526, hwirq + i=300
[ 16.125650] platform 5e00000.r5f: configured R5F for IPC-only mode
[ 16.137977] ti_sci_inta_request_resources name=:interconnect@100000:navss@30000000:interrupt-controller@33d00000, hwirq=13828540
[ 16.158753] gic_irq_domain_alloc[0] virq + i=527, hwirq + i=301
[ 16.174091] platform 5e00000.r5f: assigned reserved memory node r5f-dma-memory@a4000000
[ 16.293703] remoteproc remoteproc6: 5e00000.r5f is available
[ 16.307776] ti_sci_inta_alloc_irq 2: domain->name=:interconnect@100000:navss@30000000:interrupt-controller@33d00000, hwirq=13828540
[ 16.426024] remoteproc remoteproc5: powering up 5d00000.r5f
[ 16.431645] remoteproc remoteproc5: Booting fw image j7-main-r5f0_1-fw, size 5546248
[ 16.439556] platform 5f00000.r5f: configured R5F for IPC-only mode