This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

66AK2G12: Power Supply Connection of VPP and VPP2 pin

Part Number: 66AK2G12

Hi,

According to the data manual in Table 4-27(Power Supply Signal Descriptions),
DESCRIPTION of VPP is "leave unconnected".
However, VPP is connected to the VPP1V8 in schematic of EVMK2G(www.tij.co.jp/.../EVMK2G).
Which is correct?

If VPP needs to be connected, there is no description for VPP in data manual "5.4 Recommended Operating Conditions."
What is Recommended Operating Conditions? (1.71~1.89V?)

Also, VPP2 is only valid for high-security (66AK2G1xS) devices.
Although EVMK2G(www.tij.co.jp/.../EVMK2G) is not high-security (66AK2G1xS) devices,
VPP2 is connected to the VPP1V8 in the schematic .
Which is correct (whether the pin should be connected or not)?

Thanks.