Part Number: AM3358
Hi,
u-boot-2018.01/board/ti/am335x/mux.c
#define RXACTIVE (0x1 << 5)
#define PULLDOWN_EN (0x0 << 4) /* Pull Down Selection */
#define PULLUP_EN (0x1 << 4) /* Pull Up Selection */
#define PULLUDEN (0x0 << 3) /* Pull up enabled */
#define PULLUDDIS (0x1 << 3) /* Pull up disabled */
Why when pins configured as out put, there is no need to set PULLUP_EN?
For example below code about UART and GPIO.
static struct module_pin_mux gpio0_7_pin_mux[] = {
{OFFSET(ecap0_in_pwm0_out), (MODE(7) | PULLUDEN)}, /* GPIO0_7 */
{-1},
};
static struct module_pin_mux uart0_pin_mux[] = {
{OFFSET(uart0_rxd), (MODE(0) | PULLUP_EN | RXACTIVE)}, /* UART0_RXD */
{OFFSET(uart0_txd), (MODE(0) | PULLUDEN)}, /* UART0_TXD */
{-1},
};