Example project provided with EVM/CCS demonstrates a simple EDMA/TCC interrupt. The example will run successfully for a single run. To run a second time, it is necessary to reset the EVM. It appears that the pending interrupt is cleared in the handler. What is missing that the interrupt will not function multiple times?