Part Number: AM3352
I'm having an issue with my eth0 interface once the kernel takes over. It works perfectly in u-boot, mdio commands are all good, etc.
SDK is 06.03.00.106 and I used a slightly modified (by menuconfig) tisdk_am335x-evm_defconfig to build
The errors I get from the kernel log:
[ 1.749757] net eth0: initializing cpsw version 1.12 (0) [ 1.757608] net eth0: phy "/ocp/ethernet@4a100000/mdio@4a101000/ethernet-phy@0" not found on slave 0 [ 1.773322] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready [ 11.792520] Waiting up to 110 more seconds for network.
All the other CPSW stuff seems to go ok:
[ 1.223421] libphy: Fixed MDIO Bus: probed [ 1.302630] davinci_mdio 4a101000.mdio: davinci mdio revision 1.6, bus freq 1000000 [ 1.310367] libphy: 4a101000.mdio: probed [ 1.316095] cpsw 4a100000.ethernet: Detected MACID = f4:e1:1e:a9:af:89 [ 1.322992] cpsw 4a100000.ethernet: initialized cpsw ale version 1.4 [ 1.329405] cpsw 4a100000.ethernet: ALE Table size 1024 [ 1.334795] cpsw 4a100000.ethernet: cpts: overflow check period 500 (jiffies)
I'm thinking it's probably an issue with my fdt. I looked at several other boards with RGMII and don't see what's different. Here's the section(s) out of my dts:
cpsw_default: cpsw_default {
pinctrl-single,pins = <
/* Slave 1 */
AM33XX_IOPAD(0x914, PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* mii1_txen.rgmii1_tctl */
AM33XX_IOPAD(0x918, PIN_INPUT_PULLDOWN | MUX_MODE2) /* mii1_rxdv.rgmii1_rctl */
AM33XX_IOPAD(0x91c, PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* mii1_txd3.rgmii1_td3 */
AM33XX_IOPAD(0x920, PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* mii1_txd2.rgmii1_td2 */
AM33XX_IOPAD(0x924, PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* mii1_txd1.rgmii1_td1 */
AM33XX_IOPAD(0x928, PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* mii1_txd0.rgmii1_td0 */
AM33XX_IOPAD(0x92c, PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* mii1_txclk.rgmii1_tclk */
AM33XX_IOPAD(0x930, PIN_INPUT_PULLDOWN | MUX_MODE2) /* mii1_rxclk.rgmii1_rclk */
AM33XX_IOPAD(0x934, PIN_INPUT_PULLDOWN | MUX_MODE2) /* mii1_rxd3.rgmii1_rd3 */
AM33XX_IOPAD(0x938, PIN_INPUT_PULLDOWN | MUX_MODE2) /* mii1_rxd2.rgmii1_rd2 */
AM33XX_IOPAD(0x93c, PIN_INPUT_PULLDOWN | MUX_MODE2) /* mii1_rxd1.rgmii1_rd1 */
AM33XX_IOPAD(0x940, PIN_INPUT_PULLDOWN | MUX_MODE2) /* mii1_rxd0.rgmii1_rd0 */
>;
};
cpsw_sleep: cpsw_sleep {
pinctrl-single,pins = <
/* Slave 1 reset value */
AM33XX_IOPAD(0x914, PIN_INPUT_PULLDOWN | MUX_MODE7)
AM33XX_IOPAD(0x918, PIN_INPUT_PULLDOWN | MUX_MODE7)
AM33XX_IOPAD(0x91c, PIN_INPUT_PULLDOWN | MUX_MODE7)
AM33XX_IOPAD(0x920, PIN_INPUT_PULLDOWN | MUX_MODE7)
AM33XX_IOPAD(0x924, PIN_INPUT_PULLDOWN | MUX_MODE7)
AM33XX_IOPAD(0x928, PIN_INPUT_PULLDOWN | MUX_MODE7)
AM33XX_IOPAD(0x92c, PIN_INPUT_PULLDOWN | MUX_MODE7)
AM33XX_IOPAD(0x930, PIN_INPUT_PULLDOWN | MUX_MODE7)
AM33XX_IOPAD(0x934, PIN_INPUT_PULLDOWN | MUX_MODE7)
AM33XX_IOPAD(0x938, PIN_INPUT_PULLDOWN | MUX_MODE7)
AM33XX_IOPAD(0x93c, PIN_INPUT_PULLDOWN | MUX_MODE7)
AM33XX_IOPAD(0x940, PIN_INPUT_PULLDOWN | MUX_MODE7)
>;
};
davinci_mdio_default: davinci_mdio_default {
pinctrl-single,pins = <
/* MDIO */
AM33XX_IOPAD(0x948, PIN_INPUT_PULLUP | SLEWCTRL_FAST | MUX_MODE0) /* mdio_data.mdio_data */
AM33XX_IOPAD(0x94c, PIN_OUTPUT_PULLUP | MUX_MODE0) /* mdio_clk.mdio_clk */
>;
};
davinci_mdio_sleep: davinci_mdio_sleep {
pinctrl-single,pins = <
/* MDIO reset value */
AM33XX_IOPAD(0x948, PIN_INPUT_PULLDOWN | MUX_MODE7)
AM33XX_IOPAD(0x94c, PIN_INPUT_PULLDOWN | MUX_MODE7)
>;
};
&mac {
pinctrl-names = "default", "sleep";
pinctrl-0 = <&cpsw_default>;
pinctrl-1 = <&cpsw_sleep>;
slaves = <1>;
status = "okay";
};
&davinci_mdio {
pinctrl-names = "default", "sleep";
pinctrl-0 = <&davinci_mdio_default>;
pinctrl-1 = <&davinci_mdio_sleep>;
status = "okay";
ethphy0: ethernet-phy@0 {
compatible = "marvell";
reg = <0>;
};
};
&cpsw_emac0 {
phy-handle = <ðphy0>;
phy-mode = "rgmii-id";
};
I also went through the kernel's menuconfig and didn't see anything that jumped out at me, but the issue may also be there. I'm using a Marvell 88E1510 PHY.
Thank you!
Adam