Hi,
I'm using a customer hardware designed with AM3359 processor running with Uboot, enabled with SPI0 CS0, CLK, D0, D1 in pin mux configuration.
While accessing using sf utils in Uboot it's observed that CS pin is not getting assert to low to select the SPI flash chip. The SPI flash micron macro is enabled in uboot along with the dts.
Please help is any more configurations to be added. Thanks