This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TI DM 368 power consumption estimation



Hi :

I have a project with TI DM368 and download DM368 power consumption summary from

http://www-s.ti.com/sc/techlit/sprabb4.zip.

I feel weired about table 1 which lists core power consumption only costs 384mW.

However, core power consumption costs 920mW in table 2.

Can you explain why it differs a lot between table 1 and 2?

Which table should I use for power consumption estimation?

Because according to DM365, normal power consumption should be 1200mW to 1400mW.

I think the reasonable power consumption for DM368 should be closed to DM365, right?