I am planning ro use wifi on AM3517 , the OS is Android FroYo, Now I have downloaded the firmware into wifi module, but when start to scan the network, it could not scan any networks.Then it will unload the driver of wifi from OS. Is anybody know why? The following message is from the console when I turn on the wifi on seetings.
TIWLAN: driver init
sdioDrv_init
setting SDIO F&I clock Configuration
done setting SDIO F&I clock Configuration
tiwlan_sdio_probe
tiwlan_sdio_probe called
TIWLAN: Found TI/WLAN SDIO controller (vendor 0x104c, device 0x9066, class 0x7)
TI WiLink 1271 SDIO: Driver loaded
wlanDrvIf_Open
wlanDrvIf_Start
TIWLAN: 51.963806: pInitParams->RoamingScanning_2_4G_enable 1
TIWLAN: 52.072570: CHIP VERSION... set 1273 chip top registers
TIWLAN: 52.079589: Working on a 1273 PG 2.0 board.
TIWLAN: 52.084136: Starting to process NVS...
TIWLAN: 52.088287: No Nvs, Setting default MAC address
TIWLAN: 52.093139: pHwInit->uEEPROMCurLen: 1c
TIWLAN: 52.097259: ERROR: If you are not calibating the device, you will soon get errors !!!
TIWLAN: 52.106353: Chip ID is 0x4030111.
TIWLAN: 52.111480: FEM Type 1
TIWLAN: 52.198455: Firmware successfully downloaded.
TIWLAN: 52.203155: FW download OK...
TIWLAN: 52.230010: Firmware successfully downloaded.
TIWLAN: 52.234741: FW download OK...
TIWLAN: 52.238586: Firmware successfully downloaded.
TIWLAN: 52.243286: FW download OK...
TIWLAN: 52.249603: Firmware successfully downloaded.
TIWLAN: 52.254364: FW download OK...
TIWLAN: 52.260009: Firmware successfully downloaded.
TIWLAN: 52.264709: FW download OK...
TIWLAN: 52.269348: Finished downloading firmware.
TIWLAN: 52.273895: Firmware running.
TIWLAN: 52.293457: Firmware successfully downloaded.
TIWLAN: 52.298187: FW download OK...
TIWLAN: 52.302124:
TIWLAN: 52.303985: -----------------------------------------------------
TIWLAN: 52.310455: Driver Version : WiLink_Driver_6.1.0.0.144
TIWLAN: 52.316040: Firmware Version: Rev 6.1.0.0.335
TIWLAN: 52.320770: Station ID : 08-00-28-96-86-7E
TIWLAN: 52.325653: -----------------------------------------------------
TIWLAN: 52.332092:
TIWLAN: 52.355041: Interrogate TX/RX parameters
wlanDrvIf_Release
wlanDrvIf_Stop
tiwlan_sdio_remove
TI WiLink 1271 SDIO Driver unloaded
TI WLAN: driver unloaded