This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3354: RGB USB camera for am3354

Part Number: AM3354

Hi

I am working on custom board with am3354,  which is running with kernel 4.9. I'm looking for a USB camera which can display the recording on a lcd Display. My custom board is loaded with Opencv.  Can some one help me to find a USB camera which can be easily integrated on am3354 or any recommendations which you have already used before.

Thanks,

-Kris.

  • Hi Kris,

    In terms of USB, as long as the USB camera is UVC compliant, it will be supported in Linux kernel. Another factor to be considered is the video resolution, frame rate and format (YUV vs MPEG) which determines the max USB throughput requirement.