Hello,
We are running TIDL test bench on PSDK7.0 for TDA4x. We hare using TIDL version 06_01_02_00_09.
We have imported bin files provided to us. The bin files executed successfully in PC emulation mode for test bench.
When we try and run the same bin files using standalone testbench for Target, we get the below error :
Processing config file #0 : testvecs/config/infer/public/onnx/tidl_infer_8bit.txt Syncd Algorithm Init failed with error number: -1111 Error at line: 705 : in file src/tidl_tb.c, of function : tidlMultiInstanceTest Error Type: TIDL_E_DATAFLOW_INFO_NULL
Kindly help us identify the reason for the error seen.
Regards,
Prajakta Kulkarni