Part Number: AM5748
Customer using AM574x IDK trying to run Jailhouse + EtherCAT demo as per
Getting Fatal Excepton error using PSDK 6.03 release:
root@am57xx-evm:~# modprobe jailhouse
root@am57xx-evm:~#
root@am57xx-evm:~# jailhouse enable /usr/share/jailhouse/cells/am57xx-evm.cell
Initializing Jailhouse hypervisor v0.7 (644-g6044dcf5) on CPU 1
Code location: 0xf0000040
Page pool usage after early setup: mem 32/4074, remap 0/131072
Initializing processors:
CPU 1... OK
CPU 0... OK
Initializing unit: irqchip
Initializing unit: AM57XX
Initializing unit: PCI
Page pool usage after late setup: mem 48/4074, remap 6/131072
Activating hypervisor
[ 134.725058] The Jailhouse is opening.
root@am57xx-evm:~#
root@am57xx-evm:~# jailhouse cell create /usr/share/jailhouse/cells/am572x-ethercat.cell
Created cell "AM572X-IDK-ETHERCAT"
Page pool usage after cell creation: mem 66/4074, remap 6/131072
[ 146.597116] Created Jailhouse cell "AM572X-IDK-ETHERCAT"
root@am57xx-evm:~#
root@am57xx-evm:~# jailhouse cell load 1 /usr/share/jailhouse/inmates/ethercat_s
slave_demo.bin -a 0x90000000
Cell "AM572X-IDK-ETHERCAT" can be loaded
root@am57xx-evm:~#
root@am57xx-evm:~# jailhouse cell start 1
Started cell "AM572X-IDK-ETHERCAT"
root@am57xx-evm:~#
FATAL: instruction abort at 0x80013f00
FATAL: forbidden access (exception class 0x20)
pc=0x80013624 cpsr=0xa00001df hsr=0x80000007
r0=0x80013624 r1=0x00000001 r2=0x00000006 r3=0x00000004
r4=0x0000000f r5=0x0000001c r6=0x00000000 r7=0x80043390
r8=0x00000000 r9=0xffffffff r10=0x00000000 r11=0x00000002
r12=0x000001d3 r13=0x80043390 r14=0x90000124
Parking CPU 1 (Cell: "AM572X-IDK-ETHERCAT")