Part Number: AM3358
Other Parts Discussed in Thread: AM3359
Hi,
I am doing some initial testing with PRU Ethernet for a custom board. While I'm waiting for the custom PCB, I am using a beaglebone black to test functionality as it shares the same processor (AM3358). I am aware that the beaglebone black does not have PHYs connected to the PRU MII pins. I just want to verify that the driver is able to correctly load and create eth devices in Linux. To that end, I have patched the prueth driver init function to allow PHY-less operation (see attached patch.txt file).
I have read all the documentation about PRU Ethernet and the required device tree settings, kernel config, adding prueth-fw and pru-icss recipes from meta-ti layer to the build, etc, and have applied these changes to my yocto build (morty using ti-linux 4.19). However, when the board boots, the prueth driver complains during the probe about being unable to allocate the ocmcram it uses for passing packets back and forth. I double checked my device tree settings against those for the ICEv2 EVM (which I have running the SDK SD Image and working with PRU Ethernet) and can't find anything different with how the ocmcram is referenced.
I have attached my kernel defconfig, boot log, and device tree. Please let me know if there is anything wrong in any of them that I need to fix.
Regards,
Greg Leonberg
Booting from SD Card reading recovery ** Unable to read file recovery ** 36489 bytes read in 54 ms (659.2 KiB/s) Loaded /boot/am335x-custom.dtb from mmc 0:2 5379000 bytes read in 523 ms (9.8 MiB/s) Loaded /boot/zImage from mmc 0:2 ## Flattened Device Tree blob at 88000000 Booting using the fdt blob at 0x88000000 Loading Device Tree to 8fff4000, end 8ffffe88 ... OK Starting kernel ... [ 0.000000] Booting Linux on physical CPU 0x0 [ 0.000000] Linux version 4.19.94-custom (build_manager@custom_dev) (gcc version 6.2.0 (GCC)) #14 Tue Nov 10 10:35:00 EST 2020 [ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c5387d [ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache [ 0.000000] OF: fdt: Machine model: TI AM335x Custom [ 0.000000] Memory policy: Data cache writeback [ 0.000000] cma: Reserved 16 MiB at 0x9f000000 [ 0.000000] CPU: All CPU(s) started in SVC mode. [ 0.000000] AM335X ES2.1 (sgx neon) [ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 130048 [ 0.000000] Kernel command line: console=ttyO0,115200n8 root=/dev/mmcblk0p2 rootfstype=ext4 ro rootdelay=1 normal [ 0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes) [ 0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes) [ 0.000000] Memory: 484576K/524288K available (7330K kernel code, 641K rwdata, 2600K rodata, 372K init, 7423K bss, 23328K reserved, 16384K cma-reserved, 0K highmem) [ 0.000000] Virtual kernel memory layout: [ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB) [ 0.000000] fixmap : 0xffc00000 - 0xfff00000 (3072 kB) [ 0.000000] vmalloc : 0xe0800000 - 0xff800000 ( 496 MB) [ 0.000000] lowmem : 0xc0000000 - 0xe0000000 ( 512 MB) [ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB) [ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB) [ 0.000000] .text : 0x(ptrval) - 0x(ptrval) (7331 kB) [ 0.000000] .init : 0x(ptrval) - 0x(ptrval) ( 372 kB) [ 0.000000] .data : 0x(ptrval) - 0x(ptrval) ( 642 kB) [ 0.000000] .bss : 0x(ptrval) - 0x(ptrval) (7424 kB) [ 0.000000] Running RCU self tests [ 0.000000] NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16 [ 0.000000] IRQ: Found an INTC at 0x(ptrval) (revision 5.0) with 128 interrupts [ 0.000000] OMAP clockevent source: timer2 at 24000000 Hz [ 0.000017] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 89478484971ns [ 0.000049] clocksource: timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 79635851949 ns [ 0.000099] OMAP clocksource: timer1 at 24000000 Hz [ 0.000468] timer_probe: no matching timers found [ 0.001193] Console: colour dummy device 80x30 [ 0.001243] Lock dependency validator: Copyright (c) 2006 Red Hat, Inc., Ingo Molnar [ 0.001258] ... MAX_LOCKDEP_SUBCLASSES: 8 [ 0.001272] ... MAX_LOCK_DEPTH: 48 [ 0.001286] ... MAX_LOCKDEP_KEYS: 8191 [ 0.001300] ... CLASSHASH_SIZE: 4096 [ 0.001313] ... MAX_LOCKDEP_ENTRIES: 32768 [ 0.001327] ... MAX_LOCKDEP_CHAINS: 65536 [ 0.001340] ... CHAINHASH_SIZE: 32768 [ 0.001353] memory used by lock dependency info: 4655 kB [ 0.001367] per task-struct memory footprint: 1536 bytes [ 0.001443] Calibrating delay loop... 996.14 BogoMIPS (lpj=4980736) [ 0.078602] pid_max: default: 32768 minimum: 301 [ 0.078958] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes) [ 0.078981] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes) [ 0.080944] CPU: Testing write buffer coherency: ok [ 0.083112] Setting up static identity map for 0x80008200 - 0x80008260 [ 0.086471] devtmpfs: initialized [ 0.110649] random: get_random_u32 called from bucket_table_alloc+0x8c/0x1b0 with crng_init=0 [ 0.111005] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3 [ 0.111594] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns [ 0.111669] futex hash table entries: 256 (order: 1, 11264 bytes) [ 0.113175] pinctrl core: initialized pinctrl subsystem [ 0.117282] NET: Registered protocol family 16 [ 0.123242] DMA: preallocated 256 KiB pool for atomic coherent allocations [ 0.178593] l4_wkup_cm:clk:0010:0: failed to disable [ 0.233874] cpuidle: using governor ladder [ 0.233949] cpuidle: using governor menu [ 0.261624] OMAP GPIO hardware version 0.1 [ 0.286179] No ATAGs? [ 0.286193] hw-breakpoint: debug architecture 0x4 unsupported. [ 0.393007] edma 49000000.edma: TI EDMA DMA engine driver [ 0.397744] SCSI subsystem initialized [ 0.398711] usbcore: registered new interface driver usbfs [ 0.398956] usbcore: registered new interface driver hub [ 0.399088] usbcore: registered new device driver usb [ 0.401469] omap-mailbox 480c8000.mailbox: omap mailbox rev 0x400 [ 0.402188] Advanced Linux Sound Architecture Driver Initialized. [ 0.436910] clocksource: Switched to clocksource timer1 [ 0.567275] VFS: Disk quotas dquot_6.6.0 [ 0.567401] VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes) [ 0.616486] NET: Registered protocol family 2 [ 0.618556] tcp_listen_portaddr_hash hash table entries: 256 (order: 1, 10240 bytes) [ 0.618649] TCP established hash table entries: 4096 (order: 2, 16384 bytes) [ 0.618735] TCP bind hash table entries: 4096 (order: 5, 147456 bytes) [ 0.619298] TCP: Hash tables configured (established 4096 bind 4096) [ 0.619663] UDP hash table entries: 256 (order: 2, 20480 bytes) [ 0.619774] UDP-Lite hash table entries: 256 (order: 2, 20480 bytes) [ 0.620151] NET: Registered protocol family 1 [ 0.623876] RPC: Registered named UNIX socket transport module. [ 0.623966] RPC: Registered udp transport module. [ 0.623983] RPC: Registered tcp transport module. [ 0.623998] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 0.625495] hw perfevents: enabled with armv7_cortex_a8 PMU driver, 5 counters available [ 0.629237] Initialise system trusted keyrings [ 0.634338] workingset: timestamp_bits=30 max_order=17 bucket_order=0 [ 0.636563] NFS: Registering the id_resolver key type [ 0.636715] Key type id_resolver registered [ 0.636792] Key type id_legacy registered [ 0.636845] nfs4filelayout_init: NFSv4 File Layout Driver Registering... [ 0.644002] Key type asymmetric registered [ 0.644145] Asymmetric key parser 'x509' registered [ 0.644308] io scheduler noop registered [ 0.644330] io scheduler deadline registered [ 0.644476] io scheduler cfq registered (default) [ 0.648959] pinctrl-single 44e10800.pinmux: 142 pins, size 568 [ 0.652137] wkup_m3_ipc 44e11324.wkup_m3_ipc: could not get rproc handle [ 0.669859] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled [ 0.675956] omap_uart 44e09000.serial: no wakeirq for uart0 [ 0.676381] 44e09000.serial: ttyO0 at MMIO 0x44e09000 (irq = 30, base_baud = 3000000) is a OMAP UART0 [ 1.302082] console [ttyO0] enabled [ 1.341162] brd: module loaded [ 1.362163] loop: module loaded [ 1.367564] mtdoops: mtd device (mtddev=name/number) must be supplied [ 1.384324] libphy: Fixed MDIO Bus: probed [ 1.390070] CAN device driver interface [ 1.466965] davinci_mdio 4a101000.mdio: davinci mdio revision 1.6, bus freq 1000000 [ 1.475089] davinci_mdio 4a101000.mdio: detected phy mask fffffffe [ 1.484612] libphy: 4a101000.mdio: probed [ 1.488936] davinci_mdio 4a101000.mdio: phy[0]: device 4a101000.mdio:00, driver SMSC LAN8710/LAN8720 [ 1.499840] cpsw 4a100000.ethernet: No slave[1] phy_id, phy-handle, or fixed-link property [ 1.508718] cpsw 4a100000.ethernet: Detected MACID = 38:d2:69:49:c6:7d [ 1.517740] cpsw 4a100000.ethernet: initialized cpsw ale version 1.4 [ 1.524412] cpsw 4a100000.ethernet: ALE Table size 1024 [ 1.532754] PPP generic driver version 2.4.2 [ 1.541415] PPP BSD Compression module registered [ 1.546364] PPP Deflate Compression module registered [ 1.551772] PPP MPPE Compression module registered [ 1.556795] NET: Registered protocol family 24 [ 1.561745] usbcore: registered new interface driver rtl8150 [ 1.567883] usbcore: registered new interface driver r8152 [ 1.573733] usbcore: registered new interface driver asix [ 1.579516] usbcore: registered new interface driver ax88179_178a [ 1.585988] usbcore: registered new interface driver cdc_ether [ 1.592554] usbcore: registered new interface driver smsc75xx [ 1.598771] usbcore: registered new interface driver smsc95xx [ 1.604883] usbcore: registered new interface driver net1080 [ 1.610930] usbcore: registered new interface driver cdc_subset [ 1.617257] usbcore: registered new interface driver zaurus [ 1.623222] usbcore: registered new interface driver cdc_ncm [ 1.635698] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver [ 1.642666] ehci-omap: OMAP-EHCI Host Controller driver [ 1.648622] ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver [ 1.655342] usbcore: registered new interface driver cdc_acm [ 1.661352] cdc_acm: USB Abstract Control Model driver for USB modems and ISDN adapters [ 1.669877] usbcore: registered new interface driver cdc_wdm [ 1.675951] usbcore: registered new interface driver usb-storage [ 1.682517] usbcore: registered new interface driver usbserial_generic [ 1.689818] usbserial: USB Serial support registered for generic [ 1.696313] usbcore: registered new interface driver ftdi_sio [ 1.702485] usbserial: USB Serial support registered for FTDI USB Serial Device [ 1.710246] usbcore: registered new interface driver option [ 1.716163] usbserial: USB Serial support registered for GSM modem (1-port) [ 1.723581] usbcore: registered new interface driver usb_serial_simple [ 1.730555] usbserial: USB Serial support registered for carelink [ 1.737057] usbserial: USB Serial support registered for zio [ 1.743061] usbserial: USB Serial support registered for funsoft [ 1.749466] usbserial: USB Serial support registered for flashloader [ 1.756201] usbserial: USB Serial support registered for google [ 1.762563] usbserial: USB Serial support registered for libtransistor [ 1.769500] usbserial: USB Serial support registered for vivopay [ 1.775862] usbserial: USB Serial support registered for moto_modem [ 1.782526] usbserial: USB Serial support registered for motorola_tetra [ 1.789550] usbserial: USB Serial support registered for novatel_gps [ 1.796266] usbserial: USB Serial support registered for hp4x [ 1.802381] usbserial: USB Serial support registered for suunto [ 1.808679] usbserial: USB Serial support registered for siemens_mpi [ 1.815453] usbcore: registered new interface driver usbtest [ 1.846021] udc-core: couldn't find an available UDC - added [g_audio] to list of pending drivers [ 1.873699] mousedev: PS/2 mouse device common for all mice [ 1.885869] omap_rtc 44e3e000.rtc: registered as rtc0 [ 1.891708] i2c /dev entries driver [ 1.895430] Driver for 1-wire Dallas network protocol. [ 1.907154] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec [ 1.917534] omap_gpio 44e07000.gpio: Could not set line 6 debounce to 200000 microseconds (-22) [ 1.926645] omap_hsmmc 48060000.mmc: Got CD GPIO [ 1.933105] omap_hsmmc 48060000.mmc: Linked as a consumer to regulator.1 [ 1.969651] omap_hsmmc 481d8000.mmc: Linked as a consumer to regulator.1 [ 2.005257] ledtrig-cpu: registered to indicate activity on CPUs [ 2.014902] remoteproc remoteproc0: wkup_m3 is available [ 2.022026] remoteproc remoteproc1: 4a334000.pru is available [ 2.028331] pru-rproc 4a334000.pru: PRU rproc node pru@4a334000 probed successfully [ 2.036857] remoteproc remoteproc2: 4a338000.pru is available [ 2.043121] pru-rproc 4a338000.pru: PRU rproc node pru@4a338000 probed successfully [ 2.064256] mmc0: host does not support reading read-only switch, assuming write-enable [ 2.075166] random: fast init done [ 2.080780] mmc0: new high speed SDHC card at address b368 [ 2.089940] usbcore: registered new interface driver snd-usb-audio [ 2.097531] oprofile: using arm/armv7 [ 2.102128] Initializing XFRM netlink socket [ 2.107106] NET: Registered protocol family 10 [ 2.115232] mmcblk0: mmc0:b368 USD 7.47 GiB [ 2.127107] Segment Routing with IPv6 [ 2.131108] NET: Registered protocol family 17 [ 2.135844] NET: Registered protocol family 15 [ 2.140548] can: controller area network core (rev 20170425 abi 9) [ 2.147240] NET: Registered protocol family 29 [ 2.151901] can: raw protocol (rev 20170425) [ 2.156529] can: broadcast manager protocol (rev 20170425 t) [ 2.162774] 8021q: 802.1Q VLAN Support v1.8 [ 2.167467] Key type dns_resolver registered [ 2.172177] ThumbEE CPU extension supported. [ 2.176653] omap_voltage_late_init: Voltage driver support not added [ 2.186072] mmcblk0: p1 p2 [ 2.196131] Loading compiled-in X.509 certificates [ 2.249476] mmc1: new high speed MMC card at address 0001 [ 2.257114] mmcblk1: mmc1:0001 M62704 3.56 GiB [ 2.262371] mmcblk1boot0: mmc1:0001 M62704 partition 1 2.00 MiB [ 2.269130] mmcblk1boot1: mmc1:0001 M62704 partition 2 2.00 MiB [ 2.277858] mmcblk1rpmb: mmc1:0001 M62704 partition 3 512 KiB, chardev (246:0) [ 2.292376] mmcblk1: p1 p2 [ 2.322453] tps65217 0-0024: TPS65217 ID 0xe version 1.2 [ 2.328965] omap_i2c 44e0b000.i2c: bus 0 rev0.11 at 400 kHz [ 2.338237] remoteproc remoteproc0: powering up wkup_m3 [ 2.344297] remoteproc remoteproc0: Direct firmware load for am335x-pm-firmware.elf failed with error -2 [ 2.354464] remoteproc remoteproc0: request_firmware failed: -2 [ 2.360740] wkup_m3_ipc 44e11324.wkup_m3_ipc: rproc_boot failed [ 2.368827] hctosys: unable to open rtc device (rtc1) [ 2.375053] ALSA device list: [ 2.378283] No soundcards found. [ 2.385428] Waiting 1 sec before mounting root device... [ 3.487946] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null) [ 3.496722] VFS: Mounted root (ext4 filesystem) readonly on device 179:2. [ 3.526998] devtmpfs: mounted [ 3.530696] Freeing unused kernel memory: 372K [ 3.535348] This architecture does not have kernel memory protection. [ 3.542133] Run /sbin/init as init process INIT: version 2.88 booting Starting udev [ 4.434672] udevd[1026]: starting version 3.2 [ 4.460821] random: udevd: uninitialized urandom read (16 bytes read) [ 4.470116] random: udevd: uninitialized urandom read (16 bytes read) [ 4.477105] random: udevd: uninitialized urandom read (16 bytes read) [ 4.544146] udevd[1027]: starting eudev-3.2 [ 5.539845] prueth pruss_eth: unable to get SRAM pool [ 6.532180] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null) Error opening /dev/fb0: No such file or directory Populating dev cache [ 13.344063] random: dd: uninitialized urandom read (512 bytes read) ALSA: Restoring mixer settings... /usr/sbin/alsactl: load_state:1735: No soundcards found... Tue Nov 10 15:43:16 UTC 2020 Running postinst /etc/ipk-postinsts/000-keepalived... update-rc.d: /etc/init.d/run-postinsts exists during rc.d purge (continuing) Removing any system startup links for run-postinsts ... /etc/rcS.d/S99run-postinsts [ 14.757364] process 1 (init) attempted a POSIX timer syscall while CONFIG_POSIX_TIMERS is not set INIT: Entering runlevel: 5 Configuring network interfaces... [ 15.150222] net eth0: initializing cpsw version 1.12 (0) [ 15.157710] libphy: PHY 4a101000.mdio:01 not found [ 15.162736] net eth0: phy "4a101000.mdio:01" not found on slave 0, err -19 [ 15.169978] libphy: PHY not found [ 15.173543] net eth0: phy "" not found on slave 1, err -19 [ 15.183681] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready [ 15.189879] 8021q: adding VLAN 0 to HW filter on device eth0 eth1: ERROR while getting interface flags: No such device SIOCSIFADDR: No such device eth1: ERROR while getting interface flags: No such device SIOCSIFNETMASK: No such device SIOCADDRT: No such device eth2: ERROR while getting interface flags: No such device [ 15.691970] random: dbus-uuidgen: uninitialized urandom read (12 bytes read) [ 15.699635] random: dbus-uuidgen: uninitialized urandom read (8 bytes read) Starting system message bus: [ 16.313780] random: dbus-daemon: uninitialized urandom read (12 bytes read) dbus. Starting OpenBSD Secure Shell server: sshd generating ssh RSA key... generating ssh ECDSA key... [ 21.838232] urandom_read: 2 callbacks suppressed [ 21.838246] random: ssh-keygen: uninitialized urandom read (32 bytes read) generating ssh DSA key... generating ssh ED25519 key... done. Starting rpcbind daemon...done. Starting watchdog: [ OK ] Starting watchdog keepalive daemon: wd_keepalive. starting statd: done Starting atd: OK starting rsyslogd ... done Starting internet superserver: xinetd. * starting FTP Server: vsftpd... done. Starting crond: OK Starting network management services:pcilib: Cannot open /proc/bus/pci snmpd. custom-yocto (ARM SDK) ARM-SDK-V2.2.1 custom /dev/ttyO0 custom login: [ 34.711076] random: crng init done custom-yocto (ARM SDK) ARM-SDK-V2.2.1 custom /dev/ttyO0 custom login: root Password: root@custom:~# rmmod prueth.ko root@custom:~# find / -name "prueth.ko" /lib/modules/4.19.94-custom/kernel/drivers/net/ethernet/ti/prueth.ko root@custom:~# insmod /lib/modules/4.19.94-custom/kernel/drivers/net/ethernet/ti/prueth.ko [ 60.679538] prueth pruss_eth: unable to get SRAM pool
/dts-v1/;
#include "am33xx.dtsi"
#include "am335x-bone-common.dtsi"
#include <dt-bindings/display/tda998x.h>
/ {
model = "TI AM335x Custom";
compatible = "ti,am335x-bone-black", "ti,am335x-bone", "ti,am33xx", "custom,custom";
aliases {
ethernet1 = &pruss_emac0;
ethernet2 = &pruss_emac1;
};
leds {
pinctrl-names = "default";
pinctrl-0 = <&my_leds>;
compatible = "gpio-leds";
led2 {
label = "custom:heartbeat";
gpios = <&gpio1 12 GPIO_ACTIVE_HIGH>;
linux,default-trigger = "heartbeat";
default-state = "off";
};
led3 {
label = "custom:cpu0";
gpios = <&gpio1 13 GPIO_ACTIVE_HIGH>;
linux,default-trigger = "cpu0";
default-state = "off";
};
led4 {
label = "custom:mmc0";
gpios = <&gpio1 14 GPIO_ACTIVE_HIGH>;
linux,default-trigger = "mmc0";
default-state = "off";
};
led5 {
label = "custom:mmc1";
gpios = <&gpio1 15 GPIO_ACTIVE_HIGH>;
linux,default-trigger = "mmc1";
default-state = "off";
};
};
pruss_eth {
status = "okay";
compatible = "ti,am3359-prueth";
prus = <&pru0>, <&pru1>;
pruss = <&pruss>;
firmware-name = "ti-pruss/am335x-pru0-prueth-fw.elf",
"ti-pruss/am335x-pru1-prueth-fw.elf";
sram = <&ocmcram>;
mii-rt = <&pruss_mii_rt>;
iep = <&pruss_iep>;
interrupt-parent = <&pruss_intc>;
pinctrl-0 = <&pruss_eth_default>;
pinctrl-names = "default";
pruss_emac0: ethernet-mii0 {
phy-mode = "mii";
interrupts = <20>, <22>;
interrupt-names = "rx", "tx";
local-mac-address = [ec ec ec ec 00 01];
fixed-link {
speed = <100>;
full-duplex;
};
};
pruss_emac1: ethernet-mii1 {
phy-mode = "mii";
interrupts = <21>, <23>;
interrupt-names = "rx", "tx";
local-mac-address = [ec ec ec ec 00 02];
fixed-link {
speed = <100>;
full-duplex;
};
};
};
};
&pruss_soc_bus {
status = "okay";
};
&pruss {
status = "okay";
};
&pru0 {
status = "okay";
firmware-name = "am335x-pru0-fw";
};
&pru1 {
status = "okay";
firmware-name = "am335x-pru1-fw";
};
&am33xx_pinmux {
pruss_eth_default: pruss_eth_default {
pinctrl-single,pins = <
AM33XX_IOPAD(0x8A0, PIN_INPUT | MUX_MODE2) /* LCD_DATA0.pr1_mii_mt0_clk */
AM33XX_IOPAD(0x8A4, PIN_OUTPUT | MUX_MODE2) /* LCD_DATA1.pr1_mii0_txen */
AM33XX_IOPAD(0x8A8, PIN_OUTPUT | MUX_MODE2) /* LCD_DATA2.pr1_mii0_txd3 */
AM33XX_IOPAD(0x8AC, PIN_OUTPUT | MUX_MODE2) /* LCD_DATA3.pr1_mii0_txd2 */
AM33XX_IOPAD(0x8B0, PIN_OUTPUT | MUX_MODE2) /* LCD_DATA4.pr1_mii0_txd1 */
AM33XX_IOPAD(0x8B4, PIN_OUTPUT | MUX_MODE2) /* LCD_DATA5.pr1_mii0_txd0 */
AM33XX_IOPAD(0x8C0, PIN_INPUT | MUX_MODE5) /* LCD_DATA8.pr1_mii0_rxd3 */
AM33XX_IOPAD(0x8C4, PIN_INPUT | MUX_MODE5) /* LCD_DATA9.pr1_mii0_rxd2 */
AM33XX_IOPAD(0x8C8, PIN_INPUT | MUX_MODE5) /* LCD_DATA10.pr1_mii0_rxd1 */
AM33XX_IOPAD(0x8CC, PIN_INPUT | MUX_MODE5) /* LCD_DATA11.pr1_mii0_rxd0 */
AM33XX_IOPAD(0x8D4, PIN_INPUT | MUX_MODE5) /* LCD_DATA13.pr1_mii0_rxer */
AM33XX_IOPAD(0x8D8, PIN_INPUT | MUX_MODE5) /* LCD_DATA14.pr1_mii_mr0_clk */
AM33XX_IOPAD(0x8DC, PIN_INPUT | MUX_MODE5) /* LCD_DATA15.pr1_mii0_rxdv */
AM33XX_IOPAD(0x888, PIN_INPUT | MUX_MODE4) /* GPMC_CSn3.pr1_mii0_crs */
>;
};
};
&am33xx_pinmux {
my_leds: my_leds {
pinctrl-single,pins = <
AM33XX_IOPAD(0x830, PIN_OUTPUT_PULLDOWN | MUX_MODE7) /* gpmc_ad12.gpio1_12 */
AM33XX_IOPAD(0x834, PIN_OUTPUT_PULLDOWN | MUX_MODE7) /* gpmc_ad13.gpio1_13 */
AM33XX_IOPAD(0x838, PIN_OUTPUT_PULLDOWN | MUX_MODE7) /* gpmc_ad14.gpio1_14 */
AM33XX_IOPAD(0x83c, PIN_OUTPUT_PULLDOWN | MUX_MODE7) /* gpmc_ad15.gpio1_15 */
AM33XX_IOPAD(0x824, PIN_OUTPUT_PULLDOWN | MUX_MODE7) /* gpmc_ad9.gpio0_23 */
>;
};
};
&ldo3_reg {
regulator-min-microvolt = <1800000>;
regulator-max-microvolt = <1800000>;
regulator-always-on;
};
&mmc1 {
vmmc-supply = <&vmmcsd_fixed>;
};
&mmc2 {
vmmc-supply = <&vmmcsd_fixed>;
pinctrl-names = "default";
pinctrl-0 = <&emmc_pins>;
bus-width = <8>;
status = "okay";
};
&lcdc {
status = "disabled";
};
&usb0_phy {
status = "disabled";
};
&usb1_phy {
status = "disabled";
};
&usb0 {
status = "disabled";
};
&usb1 {
status = "disabled";
};
&spi0 {
status = "okay";
pinctrl-names = "default";
pinctrl-0 = <&spi0_pins>;
};
&am33xx_pinmux {
spi0_pins: spi0_pins {
pinctrl-single,pins = <
0x150 (PIN_INPUT_PULLUP | MUX_MODE0) /* P9.22, spi0_sclk */
0x154 (PIN_INPUT_PULLUP | MUX_MODE0) /* P9.21, spi0_d0 (miso) */
0x158 (PIN_OUTPUT_PULLUP | MUX_MODE0) /* P9.18, spi0_d1 (mosi) */
0x15c (PIN_OUTPUT_PULLUP | MUX_MODE0) /* P9.17, spi0_cs0 */
0x1a4 (PIN_OUTPUT_PULLUP | MUX_MODE7) /* crypto_nRST */
0x1b0 (PIN_INPUT_PULLUP | MUX_MODE7) /* crypto_int */
>;
};
};
&i2c0 {
clock-frequency = <400000>;
};
&i2c1 {
clock-frequency = <400000>;
};
&am33xx_pinmux {
i2c1_pins: i2c1_pins {
pinctrl-single,pins = <
AM33XX_IOPAD(0x980, SLEWCTRL_SLOW | PIN_INPUT_PULLUP | MUX_MODE3) /* UART1_RXD.I2C1_SDA */
AM33XX_IOPAD(0x984, SLEWCTRL_SLOW | PIN_INPUT_PULLUP | MUX_MODE3) /* UART1_TXD.I2C1_SCL */
>;
};
};
&i2c2 {
status = "disabled";
};
&rtc {
system-power-controller;
status = "okay";
};
&mac {
pinctrl-names = "default", "sleep";
pinctrl-0 = <&cpsw_default>;
pinctrl-1 = <&cpsw_sleep>;
slaves = <2>;
active_slave = <0>;
status = "okay";
};
&cpsw_emac0 {
phy_id = <&davinci_mdio>, <1>;
phy-mode = "rgmii";
};
&cpsw_default {
pinctrl-single,pins = <
AM33XX_IOPAD(0x910, PIN_INPUT_PULLUP | MUX_MODE2) /* mii1_rxerr.mii1_rxerr */
AM33XX_IOPAD(0x914, PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* mii1_txen.mii1_txen */
AM33XX_IOPAD(0x918, PIN_INPUT_PULLUP | MUX_MODE2) /* mii1_rxdv.mii1_rxdv */
AM33XX_IOPAD(0x91c, PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* mii1_txd3.mii1_txd3 */
AM33XX_IOPAD(0x920, PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* mii1_txd2.mii1_txd2 */
AM33XX_IOPAD(0x924, PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* mii1_txd1.mii1_txd1 */
AM33XX_IOPAD(0x928, PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* mii1_txd0.mii1_txd0 */
AM33XX_IOPAD(0x92c, PIN_INPUT_PULLUP | MUX_MODE2) /* mii1_txclk.mii1_txclk */
AM33XX_IOPAD(0x930, PIN_INPUT_PULLUP | MUX_MODE2) /* mii1_rxclk.mii1_rxclk */
AM33XX_IOPAD(0x934, PIN_INPUT_PULLUP | MUX_MODE2) /* mii1_rxd3.mii1_rxd3 */
AM33XX_IOPAD(0x938, PIN_INPUT_PULLUP | MUX_MODE2) /* mii1_rxd2.mii1_rxd2 */
AM33XX_IOPAD(0x93c, PIN_INPUT_PULLUP | MUX_MODE2) /* mii1_rxd1.mii1_rxd1 */
AM33XX_IOPAD(0x940, PIN_INPUT_PULLUP | MUX_MODE2) /* mii1_rxd0.mii1_rxd0 */
>;
};
&cpsw_sleep {
pinctrl-single,pins = <
AM33XX_IOPAD(0x910, PIN_INPUT_PULLUP | MUX_MODE7) /* mii1_rxerr.mii1_rxerr */
AM33XX_IOPAD(0x914, PIN_OUTPUT_PULLDOWN | MUX_MODE7) /* mii1_txen.mii1_txen */
AM33XX_IOPAD(0x918, PIN_INPUT_PULLUP | MUX_MODE7) /* mii1_rxdv.mii1_rxdv */
AM33XX_IOPAD(0x91c, PIN_OUTPUT_PULLDOWN | MUX_MODE7) /* mii1_txd3.mii1_txd3 */
AM33XX_IOPAD(0x920, PIN_OUTPUT_PULLDOWN | MUX_MODE7) /* mii1_txd2.mii1_txd2 */
AM33XX_IOPAD(0x924, PIN_OUTPUT_PULLDOWN | MUX_MODE7) /* mii1_txd1.mii1_txd1 */
AM33XX_IOPAD(0x928, PIN_OUTPUT_PULLDOWN | MUX_MODE7) /* mii1_txd0.mii1_txd0 */
AM33XX_IOPAD(0x92c, PIN_INPUT_PULLUP | MUX_MODE7) /* mii1_txclk.mii1_txclk */
AM33XX_IOPAD(0x930, PIN_INPUT_PULLUP | MUX_MODE7) /* mii1_rxclk.mii1_rxclk */
AM33XX_IOPAD(0x934, PIN_INPUT_PULLUP | MUX_MODE7) /* mii1_rxd3.mii1_rxd3 */
AM33XX_IOPAD(0x938, PIN_INPUT_PULLUP | MUX_MODE7) /* mii1_rxd2.mii1_rxd2 */
AM33XX_IOPAD(0x93c, PIN_INPUT_PULLUP | MUX_MODE7) /* mii1_rxd1.mii1_rxd1 */
AM33XX_IOPAD(0x940, PIN_INPUT_PULLUP | MUX_MODE7) /* mii1_rxd0.mii1_rxd0 */
>;
};
From be9d4375dae150db75ac42c633a35c3b8942c80a Mon Sep 17 00:00:00 2001
From: OpenEmbedded <oe.patch@oe>
Date: Wed, 30 Sep 2020 17:46:07 -0400
Subject: [PATCH] Add support for direct MAC fixed-type property to PRU ICSS
ethernet
---
drivers/net/ethernet/ti/prueth.c | 24 ++++++++++++++++++++++++
1 file changed, 24 insertions(+)
diff --git a/drivers/net/ethernet/ti/prueth.c b/drivers/net/ethernet/ti/prueth.c
index be3291a..8f5b355 100644
--- a/drivers/net/ethernet/ti/prueth.c
+++ b/drivers/net/ethernet/ti/prueth.c
@@ -34,6 +34,7 @@
#include "icss_mii_rt.h"
#include "icss_switch.h"
+#define NO_PHY
#define PRUETH_MODULE_VERSION "0.2"
#define PRUETH_MODULE_DESCRIPTION "PRUSS Ethernet driver"
@@ -1580,12 +1581,35 @@ static int prueth_netdev_init(struct prueth *prueth,
}
ether_addr_copy(emac->mac_addr, ndev->dev_addr);
+#ifdef NO_PHY
+ emac->phy_node = of_parse_phandle(eth_node, "phy-handle", 0);
+ if (!emac->phy_node)
+ {
+ if(!of_phy_is_fixed_link(eth_node))
+ {
+ dev_err(prueth->dev, "couldn't find fixed-link\n");
+ ret = -ENODEV;
+ goto free;
+ }
+ if(of_phy_register_fixed_link(eth_node) >= 0)
+ {
+ emac->phy_node = of_node_get(eth_node);
+ }
+ else
+ {
+ dev_err(prueth->dev, "couldn't register fixed-link\n");
+ ret = -ENODEV;
+ goto free;
+ }
+ }
+#else
emac->phy_node = of_parse_phandle(eth_node, "phy-handle", 0);
if (!emac->phy_node) {
dev_err(prueth->dev, "couldn't find phy-handle\n");
ret = -ENODEV;
goto free;
}
+#endif
emac->phy_if = of_get_phy_mode(eth_node);
if (emac->phy_if < 0) {
--
1.8.3.1