Other Parts Discussed in Thread: OMAP-L138, TMS320C6474
Dear All,
It is a general question i have, is there a possibility to use/port Linux instead of DSP/BIOS (5.x or 6.x) as RTOS to work on TI DSP processor ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: OMAP-L138, TMS320C6474
Dear All,
It is a general question i have, is there a possibility to use/port Linux instead of DSP/BIOS (5.x or 6.x) as RTOS to work on TI DSP processor ?
The short answer is yes, Linux works on a large number of embedded processors.
TI provides Linux support for some of their devices: which one are you using?
Dave
There is an active open source project to port Linux to Texas Instruments c64x family of digital signal processors and multicore devices. Go to the following Wiki site for more details:
http://linux-c6x.org/wiki/index.php/Main_Page
If you have further questions, there is a Linux-specific forum at: http://e2e.ti.com/support/embedded/f/354.aspx
Good Luck,
Dave