The build and run instructions at
software-dl.ti.com/.../index.html
were followed in order to build and run the 3D Surround View Application File Read demo app in PC emulation mode.
The app crashes shortly (<1 second) after opening a window which displays a top-down view of a vehicle.
The attached file vx_app_srv_fileio_screenshot.png is a screenshot of the window before it crashes.
Here's the app's output:
0.0s: VX_ZONE_INIT:Enabled
0.39s: VX_ZONE_ERROR:Enabled
0.47s: VX_ZONE_WARNING:Enabled
Reading calmat file
file read completed
obj->num_views = 10
APP EGL: version 1.5
Terminal setting flags:0x8a3bGL: after render_renderFrame() glError (0x501)
-----------------------------------------
In addition, how do you run the 3D Surround View Application demo in PC emulation mode?
The instructions at
software-dl.ti.com/.../group_apps_srv_demos_app_srv_camera.html
seem to be specific to the J721e EVM.
Best regards,
Deb