Other Parts Discussed in Thread: TMS320VC5410A
Hi,
We use McBSP in TMS320C5517, and config the C5517 as following:
1) In the interrupt vector definition:
_RST: .ivec reset_isr, USE_RETA; Reset / Software Interrupt #0
NMI: .ivec reset_isr ;
INT0: .ivec dummy_isr ;
INT1: .ivec dummy_isr ;
TINT0: .ivec dummy_isr ;
PROG0: .ivec dummy_isr ;
UART: .ivec dummy_isr ;
PROG1: .ivec _McBSP_RINT_Isr ;the McBSP Intrrupt receiver
...
2) EBSR = 0x0b3f; //McBSP
3)PSRCR = 8;
PRCR = 0xd0; //reset McBSP
4)set receiver interrupt in McBSP SPCRL
SPCRL = 0x20; //enable FS occur interrupt(NEWFS)
...
5) IER0 = 0x190;//enable PORG1 interrupt
IER1 = 0;
6)enable interrupt
asm(" BIT(ST1, #ST1_INTM)=#0");
When we run the program there is no interrupt when FS occur. the McBSP config and McBSP interface is the same with TMS320VC5410A which is correct with FS occur.
What should I check now?
Our CCS Version: 5.5.0.00077 .
Best Regards,
Dudechao