I would like to know if DM37x camera port can support 16-bit mode (CCIR601).
Thanks!
-Jon
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I would like to know if DM37x camera port can support 16-bit mode (CCIR601).
Thanks!
-Jon
Hi Kazunobu,
From what I understand, the DM3730 can also handle 16-bits camera data but you have to send in 8-bits at a time, double clocked, and configure the DM3730 to internally pack these bytes into a 16-bit word. Can you confirm that the 8-bit words presented to the DM3730 bus must be on CSI_D[9:2] rather than CSI_D[7:0] in order to achieve this? Thanks.
Al