We have daisy chained the UART 1's of several DSP's together. That is, Tx of one DSP to the Rx of another. There is a 22 ohm resistor between each but I would like to know if a pull up is needed?
Thanks,
Terry
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
We have daisy chained the UART 1's of several DSP's together. That is, Tx of one DSP to the Rx of another. There is a 22 ohm resistor between each but I would like to know if a pull up is needed?
Thanks,
Terry
The pull up is necessary only if you want to avoid a possible null character transmission out of reset. Since the pins are all weakly pulled down internally during reset, the receiving device might detect that as a null character. If the DSP UARTs won't be enabled until after reset then this shouldnt be an issue.
Jeff