Hi,
I try to replace the used linux source repository in arago with my own repository which hosts linux source code.
I created a bbappend-file to overwrite some variables of meta-ti/recipes-kernel/linux/linux-ti-staging_5.4.bb, which I thought it is enough.
The file looks like this:
#This will overwrite the kernel source repository URL
BRANCH = "ibg-ti-linux-5.4.y"
SRCREV = "66cf445b7697a4963cfc796e06918fe5b147fe7d"
PV = "5.4.40+git${SRCPV}"
KERNEL_GIT_URI = "git://myserver:j721e_linux/generic/ibg-linux-ti.git"
This is the error during rebuilding the image with that changed ti linux source repository:
NOTE: Executing Tasks WARNING: linux-ti-staging-5.4.40+gitAUTOINC+66cf445b76-r0a.arago5_psdkla do_fetch: Failed to fetch URL git://myserver:j721e_linux/generic/ibg-linux-ti.git;protocol=git;branch=ibg-ti-linux-5.4.y, attempting MIRRORS if available ERROR: linux-ti-staging-5.4.40+gitAUTOINC+66cf445b76-r0a.arago5_psdkla do_fetch: Fetcher failure: Fetch command export PSEUDO_DISABLED=1; unset _PYTHON_SYSCONFIGDATA_NAME; export PATH="/home/ewdt/oe/arago/sources/oe-core/scripts:/home/ewdt/oe/arago/build/arago-tmp-external-arm-glibc/work/j7_evm-linux/linux-ti-staging/5.4.40+gitAUTOINC+66cf445b76-r0a.arago5_psdkla/recipe-sysroot-native/usr/bin/aarch64-linux:/home/ewdt/oe/arago/build/arago-tmp-external-arm-glibc/work/j7_evm-linux/linux-ti-staging/5.4.40+gitAUTOINC+66cf445b76-r0a.arago5_psdkla/recipe-sysroot/usr/bin/crossscripts:/home/ewdt/oe/arago/build/arago-tmp-external-arm-glibc/work/j7_evm-linux/linux-ti-staging/5.4.40+gitAUTOINC+66cf445b76-r0a.arago5_psdkla/recipe-sysroot-native/usr/sbin:/home/ewdt/oe/arago/build/arago-tmp-external-arm-glibc/work/j7_evm-linux/linux-ti-staging/5.4.40+gitAUTOINC+66cf445b76-r0a.arago5_psdkla/recipe-sysroot-native/usr/bin:/home/ewdt/oe/arago/build/arago-tmp-external-arm-glibc/work/j7_evm-linux/linux-ti-staging/5.4.40+gitAUTOINC+66cf445b76-r0a.arago5_psdkla/recipe-sysroot-native/sbin:/home/ewdt/oe/arago/build/arago-tmp-external-arm-glibc/work/j7_evm-linux/linux-ti-staging/5.4.40+gitAUTOINC+66cf445b76-r0a.arago5_psdkla/recipe-sysroot-native/bin:/home/ewdt/oe/crosscompiletoolchain/gcc-arm-9.2-2019.12-x86_64-aarch64-none-linux-gnu/bin:/home/ewdt/oe/arago/sources/bitbake/bin:/home/ewdt/oe/arago/build/arago-tmp-external-arm-glibc/hosttools"; export HOME="/home/ewdt"; LANG=C git -c core.fsyncobjectfiles=0 clone --bare --mirror git://myserver:j721e_linux/generic/ibg-linux-ti.git /home/ewdt/oe/arago/downloads/git2/myserver.j721e_linux.generic.ibg-linux-ti.git --progress failed with exit code 128, output: Cloning into bare repository '/home/ewdt/oe/arago/downloads/git2/myserver.j721e_linux.generic.ibg-linux-ti.git'... fatal: Unable to look up myserver:j721e_linux (port 9418) (Name or service not known) ERROR: linux-ti-staging-5.4.40+gitAUTOINC+66cf445b76-r0a.arago5_psdkla do_fetch: Fetcher failure for URL: 'git://myserver:j721e_linux/generic/ibg-linux-ti.git;protocol=git;branch=ibg-ti-linux-5.4.y'. Unable to fetch URL from any source. ERROR: Logfile of failure stored in: /home/ewdt/oe/arago/build/arago-tmp-external-arm-glibc/work/j7_evm-linux/linux-ti-staging/5.4.40+gitAUTOINC+66cf445b76-r0a.arago5_psdkla/temp/log.do_fetch.29919 ERROR: Task (/home/ewdt/oe/arago/sources/meta-ti/recipes-kernel/linux/linux-ti-staging_5.4.bb:do_fetch) failed with exit code '1' NOTE: Tasks Summary: Attempted 2982 tasks of which 2981 didn't need to be rerun and 1 failed.
When I look into the logfile of the task, I noticed following:
DEBUG: Fetching software-dl.ti.com/.../git2_myserver.j721e_linux.generic.ibg-linux-ti.git.tar.gz using command '/usr/bin/env wget -t 2 -T 30 --passive-ftp --no-check-certificate -P /home/ewdt/oe/arago/downloads 'software-dl.ti.com/processor-s dk-mirror/sources/git2_myserver.j721e_linux.generic.ibg-linux-ti.git.tar.gz'' DEBUG: Fetcher accessed the network with the command /usr/bin/env wget -t 2 -T 30 --passive-ftp --no-check-certificate -P /home/ewdt/oe/arago/downloads 'software-dl.ti.com/.../git2_myserver.j721e_linux.generic.ibg-linux-ti.git.tar.gz' DEBUG: Running export PSEUDO_DISABLED=1; unset _PYTHON_SYSCONFIGDATA_NAME; export PATH="/home/ewdt/oe/arago/sources/oe-core/scripts:/home/ewdt/oe/arago/build/arago-tmp-external-arm-glibc/work/j7_evm-linux/linux-ti-staging/5.4.40+gitAUTOINC+66cf445b76-r0a.arago5_psdkla/recipe-sysroot-native/u sr/bin/aarch64-linux:/home/ewdt/oe/arago/build/arago-tmp-external-arm-glibc/work/j7_evm-linux/linux-ti-staging/5.4.40+gitAUTOINC+66cf445b76-r0a.arago5_psdkla/recipe-sysroot/usr/bin/crossscripts:/home/ewdt/oe/arago/build/arago-tmp-external-arm-glibc/work/j7_evm-linux/linux-ti-staging/5.4.40+g itAUTOINC+66cf445b76-r0a.arago5_psdkla/recipe-sysroot-native/usr/sbin:/home/ewdt/oe/arago/build/arago-tmp-external-arm-glibc/work/j7_evm-linux/linux-ti-staging/5.4.40+gitAUTOINC+66cf445b76-r0a.arago5_psdkla/recipe-sysroot-native/usr/bin:/home/ewdt/oe/arago/build/arago-tmp-external-arm-glibc/ work/j7_evm-linux/linux-ti-staging/5.4.40+gitAUTOINC+66cf445b76-r0a.arago5_psdkla/recipe-sysroot-native/sbin:/home/ewdt/oe/arago/build/arago-tmp-external-arm-glibc/work/j7_evm-linux/linux-ti-staging/5.4.40+gitAUTOINC+66cf445b76-r0a.arago5_psdkla/recipe-sysroot-native/bin:/home/ewdt/oe/crossc ompiletoolchain/gcc-arm-9.2-2019.12-x86_64-aarch64-none-linux-gnu/bin:/home/ewdt/oe/arago/sources/bitbake/bin:/home/ewdt/oe/arago/build/arago-tmp-external-arm-glibc/hosttools"; export HOME="/home/ewdt"; /usr/bin/env wget -t 2 -T 30 --passive-ftp --no-check-certificate -P /home/ewdt/oe/arago/ downloads 'software-dl.ti.com/.../git2_myserver.j721e_linux.generic.ibg-linux-ti.git.tar.gz' --progress=dot -v --2020-11-16 14:53:15-- software-dl.ti.com/.../git2_myserver.j721e_linux.generic.ibg-linux-ti.git.tar.gz Resolving software-dl.ti.com (software-dl.ti.com)... 184.30.209.167, 2a02:26f0:1500:18f::b48, 2a02:26f0:1500:1a6::b48 Connecting to software-dl.ti.com (software-dl.ti.com)|184.30.209.167|:80... connected. HTTP request sent, awaiting response... 404 Not Found 2020-11-16 14:53:15 ERROR 404: Not Found.
I noticed this: Fetching 
So it seems that KERNEL_GIT_URI seems to get wrapped into some TI specific paths to get the source code.
Can you guide me how to successfully replace the TI linux kernel source repository, with my own git repository?
Best regards,
Thomas