Hi,
I am using CCS4 V2.2 with bios version bios_6_30_03_46. I have been searching on how to do memory overlay in the configuration file, but I couldn't find anything. Is there any possible way to do memory section overlay using the configuration file? For example, I have two memory sections that I placed in DDR2 as follow, how can I make them such that the two memory sections will share the same DDR2 starting address.
Program.sectMap[".sect_a"] = "DDR2";
Program.sectMap[".sect_b"] = "DDR2";
In another word how can I join them as a union similar to what I have done in the past in CCSV3
UNION: run = DDR2
{
.sect_a: {}
.sect_b: {}
}
Also can I explicitly force a a.lib file into a particular memory using the configuration file?
Thanks in advance,
Dominic