Part Number: TDA4VM
Hi Experts
We made own custom board but when running the S/W, system is hanged frequently in the middle of linux booting( Data Abort, Kernel Panic etc)
Rare case, can boot and see the camera image.
we are using SD_card boot and with same software, EVM works fine.
Software Version is
RTOS : rtos_07_00_00_11
Linux : ti-processor-sdk-linux-automotive-j7-evm-07_00_01
Even we are using same LPDDR4(MT53D1024M32D4DT) with EVM, I think this issue is related to the LPDDR4 PCB layout.
My Questions are :
1. Can you provide us LPDDR4 configuration tool
2. How can we slow down the LPDDR4 clock frequency
Thanks In Advance
Hennessy