This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Boot WinCE6 from NAND flash on AM1808 EVM

Other Parts Discussed in Thread: OMAPL138

TI,

In the “Windows Embedded CE 6.0 BSP for the OMAP-L13x/AM17x/AM18x User Guide” chapter 6.2 “EBOOT Features” it is stated:

The EBOOT implementation supports the following functionality:

…

-  Flashing of CE images to NAND, NOR (OMAPL138_AM18X only)

-  Boot CE image from NAND, NOR (OMAPL138_AM18X only), SD/MMC card

Is there a procedure available that describes flashing a CE image onto NAND flash and then subsequently booting the CE image from the NAND flash?

Best,

Nelson