I try to connect a Low speed and/or Full speed device to HSUSB Host port of the AM/DM37x EVM, but it always reports "hub 1-0:1.0: Cannot enable port 2. Maybe the USB cable is bad?" Then I try to attached the devics through a High speed USB hub, it can detect them without problem.
Is this a hardware issue because of using SMSC USB3320 physical? Or the HSUSB driver has problem to support Full and Low speed device? Or there is a update of the linux kernel SDK that has solved this problem?
Regards,
Colman